AHAB: status information and user space tools

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

AHAB: status information and user space tools

跳至解决方案
3,320 次查看
OlegHahm
Contributor I

Hi!

I'm currently developing a secure boot solution for one of our customers. Following some tutorials (including the ones provided by U-Boot itself), I've managed to get a signed version of U-Boot to execute on my iMX.8 Quad Plus.

Since I haven't programmed the fuses yet, I get a message like

Lifecycle: 0x0020, NXP closed

SECO Event[0] = 0x0087FA00
        CMD = AHAB_AUTH_CONTAINER_REQ (0x87)
        IND = AHAB_BAD_KEY_HASH_IND (0xFA)

SECO Event[1] = 0x0087FA00
        CMD = AHAB_AUTH_CONTAINER_REQ (0x87)
        IND = AHAB_BAD_KEY_HASH_IND (0xFA)

sc_seco_get_event: idx: 2, res:3

when calling ahab_status from the U-Boot CLI.

Now I wonder if there's any documentation on this output and if there are any Linux user space tools to read the SECO information.

 

标记 (1)
0 项奖励
回复
1 解答
3,306 次查看
Yuri
NXP Employee
NXP Employee

@OlegHahm 
Hello,

  According to the following

https://www.digi.com/resources/documentation/digidocs/embedded/dey/2.6/cc8x/yocto-trustfence_t_secur...

"For the command field (CMD), the expected value at this step is 0x87 (ID for AHAB_AUTH_CONTAINER_REQ). The indicator field (IND) shows the code AHAB_BAD_KEY_HASH_IND (0xFA) because the key hash verification does not match the current OTPs. Once the OTP SRK hash fuses are programmed on the target OTPs, the AHAB events will no longer have errors.

See the NXP secure boot application notes for more information on event decoding."

 

 Please use section 4.3 (Verifying/Decoding SECO events) of AN12312 (Secure Boot
on i.MX 8 and i.MX 8X Families using AHAB).

https://www.nxp.com/webapp/Download?colCode=AN12312

 

Regards,
Yuri.

在原帖中查看解决方案

3 回复数
3,307 次查看
Yuri
NXP Employee
NXP Employee

@OlegHahm 
Hello,

  According to the following

https://www.digi.com/resources/documentation/digidocs/embedded/dey/2.6/cc8x/yocto-trustfence_t_secur...

"For the command field (CMD), the expected value at this step is 0x87 (ID for AHAB_AUTH_CONTAINER_REQ). The indicator field (IND) shows the code AHAB_BAD_KEY_HASH_IND (0xFA) because the key hash verification does not match the current OTPs. Once the OTP SRK hash fuses are programmed on the target OTPs, the AHAB events will no longer have errors.

See the NXP secure boot application notes for more information on event decoding."

 

 Please use section 4.3 (Verifying/Decoding SECO events) of AN12312 (Secure Boot
on i.MX 8 and i.MX 8X Families using AHAB).

https://www.nxp.com/webapp/Download?colCode=AN12312

 

Regards,
Yuri.

3,299 次查看
OlegHahm
Contributor I

Thanks for the pointer, this is helpful indeed. However, I'm still wondering if there is a way to retrieve the AHAB status information from within Linux (not U-Boot). Do you have any idea?

0 项奖励
回复
3,297 次查看
Yuri
NXP Employee
NXP Employee

@OlegHahm 
Hello,

  we do not have such utility for Linux user space

Regards,
Yuri.