ADV7180 probing issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADV7180 probing issue

498 Views
purvi_billore1
Contributor III

Working on i.Mx6q based custom board. The kernel log shows following,

V4L2 device 'Mxc Camera' on IPU1_CSI0 registered as video0
ERROR: v4l2 capture: slave not found!

The ADV180 decoder worked when /unit_test/mxc_v4l2_tvin.out  run through command line. The video displayed on the screen. When simple opencv application of capturing video run, shows following error.
ERROR: v4l2 capture: slave not found!

Thanks and Regards,

Purvi Billore

0 Kudos
1 Reply

423 Views
igorpadykov
NXP Employee
NXP Employee

Hi Purvi

if ADV180 decoder worked  fine with v4l2_tvin.out probably

there are problems with image, one can try to rebuild all from scratch

including opencv application.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos