ADMA not working on imx6sl?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADMA not working on imx6sl?

Jump to solution
1,516 Views
xlin
Contributor III

Hi,

I heard from about that there is an issue with ADMA on imx6sl. if any of you knows this issue, would you please shed light on it?  Is this issue  imx6sl-only?

Thanks,

Xinsi Lin

Labels (3)
0 Kudos
Reply
1 Solution
1,335 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xinsi

it is working except that ADMA can not be used with

SDIO2.0/SDIO3.0 cards, due to ERR004536 IMX6SLCE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,336 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xinsi

it is working except that ADMA can not be used with

SDIO2.0/SDIO3.0 cards, due to ERR004536 IMX6SLCE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply