ADC with DMA in imx91

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC with DMA in imx91

1,812件の閲覧回数
sbmd_1234
Contributor III

Hi NXP Team,


I am new to working with ADC and I wanted to implement the DMA with ADC please tell me how to implement it on the imx91 processor.


Thanks.

0 件の賞賛
返信
7 返答(返信)

1,773件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Default driver doesn't support DMA feature, please refer RM to configure DMA registers, DMAE, and DMARn, for different channel groups.


Best Regards
Zhiming

0 件の賞賛
返信

1,694件の閲覧回数
sbmd_1234
Contributor III

Hi,

Do you have any reference code, or document that would be helpful for the DMA implementation with ADC.

Thanks for your help!

0 件の賞賛
返信

1,682件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

I don't find such reference code in doucument.


Best Regards,
Zhiming

0 件の賞賛
返信

1,672件の閲覧回数
sbmd_1234
Contributor III

Hi,

How can we know the sample rate used in ADC and also if we want to configure for 200k samples per second then how could we do that?


Thanks.

0 件の賞賛
返信

1,639件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

Checked with SW team , they don't have plan to add DMA feature for ADC.

The adc driver has integrated with iio sensor framework, you can refer below link to access this device to get/set data you want with /sys/bus/iio/iio:deviceX/.

https://developer.toradex.com/linux-bsp/application-development/peripheral-access/adc-linux/



Best Regards,
Zhiming

0 件の賞賛
返信

1,627件の閲覧回数
sbmd_1234
Contributor III

Hi @Zhiming_Liu ,

Actually my concern is that I can read the ADC value as /sys/bus/iio/devices/iio:device0/in_voltage0_raw, but how can we read the desired samples per second for example I need 200k samples per second how can I read or implement.

Please help with this.

Thanks.

0 件の賞賛
返信

1,590件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

The driver doesn't support iio buffer and iio scan feature, you may need refer other adc driver like drivers/iio/adc/ad7768-1.c to add them.

Best Regards,
Zhiming

0 件の賞賛
返信