ADC with DMA in imx91

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC with DMA in imx91

1,781 次查看
sbmd_1234
Contributor III

Hi NXP Team,


I am new to working with ADC and I wanted to implement the DMA with ADC please tell me how to implement it on the imx91 processor.


Thanks.

0 项奖励
回复
7 回复数

1,742 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Default driver doesn't support DMA feature, please refer RM to configure DMA registers, DMAE, and DMARn, for different channel groups.


Best Regards
Zhiming

0 项奖励
回复

1,663 次查看
sbmd_1234
Contributor III

Hi,

Do you have any reference code, or document that would be helpful for the DMA implementation with ADC.

Thanks for your help!

0 项奖励
回复

1,651 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

I don't find such reference code in doucument.


Best Regards,
Zhiming

0 项奖励
回复

1,641 次查看
sbmd_1234
Contributor III

Hi,

How can we know the sample rate used in ADC and also if we want to configure for 200k samples per second then how could we do that?


Thanks.

0 项奖励
回复

1,608 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

Checked with SW team , they don't have plan to add DMA feature for ADC.

The adc driver has integrated with iio sensor framework, you can refer below link to access this device to get/set data you want with /sys/bus/iio/iio:deviceX/.

https://developer.toradex.com/linux-bsp/application-development/peripheral-access/adc-linux/



Best Regards,
Zhiming

0 项奖励
回复

1,596 次查看
sbmd_1234
Contributor III

Hi @Zhiming_Liu ,

Actually my concern is that I can read the ADC value as /sys/bus/iio/devices/iio:device0/in_voltage0_raw, but how can we read the desired samples per second for example I need 200k samples per second how can I read or implement.

Please help with this.

Thanks.

0 项奖励
回复

1,559 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

The driver doesn't support iio buffer and iio scan feature, you may need refer other adc driver like drivers/iio/adc/ad7768-1.c to add them.

Best Regards,
Zhiming

0 项奖励
回复