ADC input pin of i.MX 6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC input pin of i.MX 6ULL

345件の閲覧回数
simon_ko
Contributor III

1.

I know that the ADC of i.MX 6ULL can receive 10 inputs.

However, in the Reference Manual of i.MX 6ULL, in External Signals of the ADC Chapter, 15 pins are additionally described in addition to the 10 pins.

Page 394~395 of IMX6ULLRM Rev.1 contains the relevant contents.

Please check which one is correct.

 

2. 

In the ADC block diagram of IMX6ULLRM Rev.1, there is ADC Input as MUX Input.
There are only ADC1_IN0, ADC1_IN1, ..., ADC2_IN3, is it a simple typo?
How to use ADC2_IN4~9?

 

 

0 件の賞賛
返信
0 返答(返信)