ADC input pin of i.MX 6ULL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC input pin of i.MX 6ULL

343 次查看
simon_ko
Contributor III

1.

I know that the ADC of i.MX 6ULL can receive 10 inputs.

However, in the Reference Manual of i.MX 6ULL, in External Signals of the ADC Chapter, 15 pins are additionally described in addition to the 10 pins.

Page 394~395 of IMX6ULLRM Rev.1 contains the relevant contents.

Please check which one is correct.

 

2. 

In the ADC block diagram of IMX6ULLRM Rev.1, there is ADC Input as MUX Input.
There are only ADC1_IN0, ADC1_IN1, ..., ADC2_IN3, is it a simple typo?
How to use ADC2_IN4~9?

 

 

0 项奖励
回复
0 回复数