ADC input pin of i.MX 6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC input pin of i.MX 6ULL

342 Views
simon_ko
Contributor III

1.

I know that the ADC of i.MX 6ULL can receive 10 inputs.

However, in the Reference Manual of i.MX 6ULL, in External Signals of the ADC Chapter, 15 pins are additionally described in addition to the 10 pins.

Page 394~395 of IMX6ULLRM Rev.1 contains the relevant contents.

Please check which one is correct.

 

2. 

In the ADC block diagram of IMX6ULLRM Rev.1, there is ADC Input as MUX Input.
There are only ADC1_IN0, ADC1_IN1, ..., ADC2_IN3, is it a simple typo?
How to use ADC2_IN4~9?

 

 

0 Kudos
Reply
0 Replies