Hi all
Please tell me memory map of i.MX7D.
Accroding to the section 2.1.2 Cortex-A7 Memory Map of IMX7DRM Rev. 0.1, 08/2016, the memory map has TCM region as follow.
Q1.
Is it a different TCM which is inplemented to M4 ?
Q2.
If Q1 is yes, could you provide me a block diagram which shows connection with A7 ?
I want to know the connection whether it connect bia L1 cache and L2 cache or not.
Q3.
If Q1 is no, can A7 access to the TCM ?
Ko-hey
Hello,
CA7 core of i.MX7 can access TCM of CM4 via CA7 memory area,
shown in Cortex-A7 Memory Map .
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct
Answer button. Thank you!
------------------------------------------------------------------------------