A problem about compiling u-boot for imx6q_rom-3420

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

A problem about compiling u-boot for imx6q_rom-3420

1,437 次查看
hanshan
Contributor II

Hello,

  When I compiled my u-boot for imx6q_rom-3420,I came cross a problem, the log is printed as follows.And anybody who can help me  to compile my u-boot?Thanks very much.

Adv-Boot 2009.08-advantech_rom3420_1G_V2.210_svn414 (Mar 14 2014 - 09:51:19)
U-Boot 2009.08-dirty (Nov 18 2016 - 17:40:28)
CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 181
Temperature: 53 C, calibration data 0x5784e369
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-ROM-3420: unknown-board Board: 0x63012 [POR ]
Boot Device: SPI NOR
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1
JEDEC ID: 0x20:0xba:0x16
In: serial
Out: serial
Err: serial
boardcfg_get_mac
JEDEC ID: 0x20:0xba:0x16
MAC addr = 0x00:0x19:0x0F:0x17:0x00:0xFF
Net: got MAC address from IIM: 00:00:00:00:00:00
FEC0
booting from iNAND
Hit any key to stop autoboot: 0
MX6Q ROM-3420 U-Boot > run bootcmd
mmc1(part 0) is current device
Unknown command 'if' - try 'help'
Unknown command 'then' - try 'help'
Unknown command 'then' - try 'help'
Unknown command 'else' - try 'help'
Unknown command 'then' - try 'help'
Unknown command 'else' - try 'help'
Unknown command 'fi' - try 'help'
Unknown command 'fi' - try 'help'
Unknown command 'else' - try 'help'
Unknown command 'fi' - try 'help'
MX6Q ROM-3420 U-Boot >
标签 (2)
标记 (2)
2 回复数

1,253 次查看
igorpadykov
NXP Employee
NXP Employee

Hi han

please set valid uboot environmental variables with setenv command

and read board manual sect.3.4.1 Build u-boot Image, setenv bootargs sect.3.8.5
http://advdownload.advantech.com/productfile/Downloadfile1/1-Y0QMII/ROM-3420_USER_MANUAL_ED.2-FINAL....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,253 次查看
hanshan
Contributor II

Thank u for your reply !!I have soled this problem under your help!!

0 项奖励
回复