A probability of USB hub failure when a 3.0 udisk was inserted on custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A probability of USB hub failure when a 3.0 udisk was inserted on custom board

861件の閲覧回数
zhengguang_yang
Contributor II
When the system is booted with a 3.0 udisk was inserted on my board, there will be a probability of USB hub failure. When this happens, all USB interfaces from HUB can't be used.
Normal:
# lsusb
Bus 001 Device 005: ID 0951:1666
Bus 001 Device 002: ID 0424:2517
Bus 001 Device 001: ID 1d6b:0002
Abnormal:
# lsusb
Bus 001 Device 002: ID 0424:2517
Bus 001 Device 001: ID 1d6b:0002
SW version as follows:
BSP version :Yocto 2.1 
Kernel version: 4.1.15
But there is no such phenomenon on Yocto 1.8(Kernel version:3.14.52).
ラベル(1)
0 件の賞賛
返信
1 返信

784件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

what bsp used in the case, one can try with nxp official Demo Images from link

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信