Hello,
I am trying to get the my 8M Mini EVKB board to display to my monitor via the MIPI to HDMI adaptor provided. I was having issues with uboot so I decided to do a fresh image from NXP (specifically android-11.0.0_2.0.0_image_8mmevk). However, after switching into Serial Download Mode on the dip switches, UUU would not recognize the board. I'm using Windows 10 and in Device Manager the USB connection is recognized on two of the COM ports (COM 5 & 6 for my laptop). I've already tried pushing through with the flash, but all I get is the Wait for a Recognizable Device.
I switched back to eMMC mode to check if the terminal would still work through PUTTY and the device still responds.
Any Idea what to do? I've searched the forum and all the advice is typically check the power supply (for both the board and monitor), switch is ON, and make sure the dip switches are correct (first four are 1010 and last is 0). I've confirmed those tips and I now need more in-depth advice than that.
Connected State shown here: https://community.nxp.com/t5/i-MX-Processors/uuu-tool-does-not-recognize-the-connected-board/m-p/116...
Solved! Go to Solution.
Good News. I have figured out my own problems.
I admit these were dumb mistakes, but I also would say that the Quick Start Guide included with the board isn't very deep especially when it comes to troubleshooting. I'd check the Android Quick-Start guide for issues with flashing. Looking around uboot and UUU (Pronounced 3U or U^3 ?) can also help (uboot can be accessed by using the debug serial monitor right when power is turned on).
Good News. I have figured out my own problems.
I admit these were dumb mistakes, but I also would say that the Quick Start Guide included with the board isn't very deep especially when it comes to troubleshooting. I'd check the Android Quick-Start guide for issues with flashing. Looking around uboot and UUU (Pronounced 3U or U^3 ?) can also help (uboot can be accessed by using the debug serial monitor right when power is turned on).