8Gbit DDR3 on i.MX6 Quad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8Gbit DDR3 on i.MX6 Quad

Jump to solution
647 Views
motting
Contributor I

We are planning to start a project that using i.MX 6Quad.

Due to the size limitation, our PCB may only have space for 2 DRAM chips.

We want to maximize the memory so we expect to put 2pcs Micron 8Gbit (512Mx16) DDR3 DRAMs (32bit, 2GB memory).

Does i.MX 6Quad supports this configuration?

The spec of i.MX 6Quad does say it supports up to 4GB but we are not sure if it supports it in 512Mx1x32.

Thanks.

Labels (2)
0 Kudos
1 Solution
529 Views
igorpadykov
NXP Employee
NXP Employee

Hi Motti

supported ddr3 configurations (row:11-16, column: 9-12 ) can be found in

sect.44.12.1 MMDC Core Control Register (MMDCx_MDCTL) i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
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
530 Views
igorpadykov
NXP Employee
NXP Employee

Hi Motti

supported ddr3 configurations (row:11-16, column: 9-12 ) can be found in

sect.44.12.1 MMDC Core Control Register (MMDCx_MDCTL) i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos