88W8997 wifi and BT test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

88W8997 wifi and BT test

584 Views
sam_yu
Contributor I

Use IMX8M to drive 88W8997 with wlan: version=SD8997---16.92.21. p84.4-MM5X16391. p3-GPL - (FP92), and use the following instructions to test the 5GRF parameters

Echo "rf_test_mode=1">/proc/mwlan/adapter0/config

Echo "rx_antenna=3">/proc/mwlan/adapter0/config

Echo "tx_antenna=3">/proc/mwlan/adapter0/config

Echo "band=1">>/proc/mwlan/adapter0/config

Echo "tx_power=10 2 2">/proc/mwlan/adapter0/config

Echo "tx_continuous=1 1 0xAAA 0 3 7">/proc/mwlan/adapter0/config

The power configuration is 10dbm, but the test result is -7.3dbm, but the 2.4G test is normal. Do you need to configure other parameters????

Labels (1)
0 Kudos
Reply
0 Replies