7ulp imx-yocto-L5.10.52_2.1.0 build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

7ulp imx-yocto-L5.10.52_2.1.0 build

7,875 Views
Anonymous
Deactivated User

HI. all

I am porting imx-yocto-L5.10.52_2.1.0 with 7ulp evk.

From last Friday, when building yocto, the following error message is displayed and the build fails.

The same goes for the link to the yocto user guide document in 5.10.52_2.1.0.

If you know a solution, please share.

If you look at the contents, they are all related to qt5.

=================================================================
WARNING: qtbase-native-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Failed to fetch URL git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.15.2;protocol=git, attempting MIRRORS if available
WARNING: qtdeclarative-native-5.15.2+gitAUTOINC+104eae5b17-r0 do_fetch: Failed to fetch URL git://code.qt.io/qt/qtdeclarative.git;name=qtdeclarative;branch=5.15.2;protocol=git, attempting MIRRORS if available
ERROR: qtdeclarative-native-5.15.2+gitAUTOINC+104eae5b17-r0 do_fetch: Fetcher failure: Unable to find revision 104eae5b17b0ec700391e9539ee3a4f638588194 in branch 5.15.2 even from upstream
ERROR: qtdeclarative-native-5.15.2+gitAUTOINC+104eae5b17-r0 do_fetch: Fetcher failure for URL: 'git://code.qt.io/qt/qtdeclarative.git;name=qtdeclarative;branch=5.15.2;protocol=git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/hkkim/workspace/c4_job/c4-rcs-halo-remote-manifest/buildhalo/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/temp/log.do_fetch.1672358
ERROR: Task (virtual:native:/home/hkkim/workspace/c4_job/c4-rcs-halo-remote-manifest/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_git.bb:do_fetch) failed with exit code '1'
WARNING: qtdeclarative-5.15.2+gitAUTOINC+104eae5b17-r0 do_fetch: Failed to fetch URL git://code.qt.io/qt/qtdeclarative.git;name=qtdeclarative;branch=5.15.2;protocol=git, attempting MIRRORS if available
ERROR: qtdeclarative-5.15.2+gitAUTOINC+104eae5b17-r0 do_fetch: Fetcher failure: Unable to find revision 104eae5b17b0ec700391e9539ee3a4f638588194 in branch 5.15.2 even from upstream
ERROR: qtdeclarative-5.15.2+gitAUTOINC+104eae5b17-r0 do_fetch: Fetcher failure for URL: 'git://code.qt.io/qt/qtdeclarative.git;name=qtdeclarative;branch=5.15.2;protocol=git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/hkkim/workspace/c4_job/c4-rcs-halo-remote-manifest/buildhalo/tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/qtdeclarative/5.15.2+gitAUTOINC+104eae5b17-r0/temp/log.do_fetch.1689244
ERROR: Task (/home/hkkim/workspace/c4_job/c4-rcs-halo-remote-manifest/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_git.bb:do_fetch) failed with exit code '1'
ERROR: qtbase-native-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Fetcher failure: Unable to find revision 40143c189b7c1bf3c2058b77d00ea5c4e3be8b28 in branch 5.15.2 even from upstream
ERROR: qtbase-native-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Fetcher failure for URL: 'git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.15.2;protocol=git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/hkkim/workspace/c4_job/c4-rcs-halo-remote-manifest/buildhalo/tmp/work/x86_64-linux/qtbase-native/5.15.2+gitAUTOINC+40143c189b-r0/temp/log.do_fetch.1615753
ERROR: Task (/home/hkkim/workspace/c4_job/c4-rcs-halo-remote-manifest/sources/meta-qt5/recipes-qt/qt5/qtbase-native_git.bb:do_fetch) failed with exit code '1'
WARNING: qtbase-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Failed to fetch URL git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.15.2;protocol=git, attempting MIRRORS if available
ERROR: qtbase-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Fetcher failure: Unable to find revision 40143c189b7c1bf3c2058b77d00ea5c4e3be8b28 in branch 5.15.2 even from upstream
ERROR: qtbase-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Fetcher failure for URL: 'git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.15.2;protocol=git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/hkkim/workspace/c4_job/c4-rcs-halo-remote-manifest/buildhalo/tmp/work/cortexa7t2hf-neon-mx7ulp-poky-linux-gnueabi/qtbase/5.15.2+gitAUTOINC+40143c189b-r0/temp/log.do_fetch.1630035
ERROR: Task (/home/hkkim/workspace/c4_job/c4-rcs-halo-remote-manifest/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1576 tasks of which 0 didn't need to be rerun and 4 failed.
 
 
 
 
 
 
 
 
0 Kudos
Reply
12 Replies

7,232 Views
alberto_alvarez
NXP Employee
NXP Employee

Hello @Anonymous,

I ran into the same issue when building LF5.10.72_2.2.0. Unfortunately, the original repository has been removed. A better fix to this issue is to move to this available mirror for fetching: https://gitlab.com/qtmirror/qtbase/-/tree/5.15.2

You can find the needed patch attached. Use this as a better workaround.

Best regards,

Alberto

7,820 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Anonymous 

Check if you can download it by "git clone git://code.qt.io/qt/qtbase.git"

If not, you need to fix the network security, or change the git protocol to https accordingly.

 

Best regards

Harvey

Tags (1)
0 Kudos
Reply

7,815 Views
Anonymous
Deactivated User

There is nothing wrong with the git clone you gave me.

0 Kudos
Reply

7,698 Views
Anonymous
Deactivated User

It seems to me that this is not a server issue.
How should I fix it?

I am following your guide.
When a customer raises an issue, it is reviewed and checked to see if it works or not.
The solution must be disclosed.

have you tried building it?

0 Kudos
Reply

7,839 Views
paolamg
Contributor II

@Anonymous 

 

Just to try... I edited qt5-git.inc adding ";nobranch=1" and the fetch passes

SRC_URI = " \
${QT_GIT}/${QT_MODULE}.git;name=${QT_MODULE};${QT_MODULE_BRANCH_PARAM};protocol=${QT_GIT_PROTOCOL};nobranch=1 \
"

Now I have to move this modification in my local.conf:

QT_MODULE_BRANCH_PARAM_append = ";nobranch=1"

 

5,816 Views
paolamg
Contributor II

Now it's official:

https://github.com/nxp-imx/meta-imx/commit/2a816fb427a1e84a898d1c6ea2518b48b5cd12ef

NXP updated the manifest too:

https://github.com/nxp-imx/imx-manifest/blob/imx-linux-hardknott/imx-5.10.35-2.0.0.xml

...

<project name="meta-imx" path="sources/meta-imx" remote="nxp-imx" revision="refs/tags/rel_imx_5.10.35_2.0.0_gh" upstream="hardknott-5.10.35-2.0.0">

...

@Anonymous @jgrider @Danube 

0 Kudos
Reply

7,576 Views
Anonymous
Deactivated User

As you said, I also succeeded in the build.
thank you
However, application development with QT5 may be unstable because all fetch contents are not applied.

What I'm complaining about is NXP's attitude.
If NXP guides the customer, of course they should tell the solution.

0 Kudos
Reply

7,578 Views
jgrider
Contributor II

This worked for me when I had the same issue.  Thank you.

7,845 Views
paolamg
Contributor II

Hello,
I'm, getting the same error, building https://source.codeaurora.org/external/imx/imx-manifest/tree/imx-5.10.35-2.0.0.xml?h=imx-linux-hardk...

WARNING: qtbase-native-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Failed to fetch URL git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.15.2;protocol=git, attempting MIRRORS if available
ERROR: qtbase-native-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Fetcher failure: Unable to find revision 40143c189b7c1bf3c2058b77d00ea5c4e3be8b28 in branch 5.15.2 even from upstream
ERROR: qtbase-native-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Fetcher failure for URL: 'git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.15.2;protocol=git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /tmp/work/tmp/work/x86_64-linux/qtbase-native/5.15.2+gitAUTOINC+40143c189b-r0/temp/log.do_fetch.668468
ERROR: Task (/tmp/sources/meta-qt5/recipes-qt/qt5/qtbase-native_git.bb:do_fetch) failed with exit code '1'

0 Kudos
Reply

7,543 Views
Danube
Contributor IV

Hi

 

add

QT_MODULE_BRANCH_PARAM_append = ";nobranch=1"

in local.conf

 

0 Kudos
Reply

7,535 Views
paolamg
Contributor II
it's what I suggested...

7,431 Views
jgrider
Contributor II

Thank you @paolamg, you're the hero we need, not the one we deserve. 

0 Kudos
Reply