7" LVDS, LCD Display with resistive touch panel for SABRE AI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

7" LVDS, LCD Display with resistive touch panel for SABRE AI

Jump to solution
1,341 Views
jeevanmahadevu
Contributor II

Hello,

We have ordered the SABRE AI development board and we want to connect 7" LCD with resistive touch using LVDS interface to the development board.

Please suggest the compatible LCD which can be used for the development board.

Thank you.

Tags (1)
0 Kudos
1 Solution
873 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
2 Replies
874 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
873 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeevan

as for lvds LCD, only HannStar LVDS panel is supported in BSP

as described in i.MX_6Dual6Quad_SABRE-AI_Linux_Release_Notes.pdf

L3.0.35_4.1.0_LINUX_DOCS

Some 7' LCDs are ported to i.MX6 BSPs, for example refer below

http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------