Hi Jemish,
I searched for the LCD part number that you mentioned, but I wasn’t able to find related information.
Regarding i.MX6 side, you may be more specific which member of the i.MX6 family is intended to be used.
Anyway, as a general advice for LCD screens with fewer color pins, they will affect the amount of different colors capable of be shown by the LCD. For example, a 24-bits LCD on 888 configuration will have 8 bits per color (RGB) up to 16M colors, while 16-bits may be 565 configuration up to 65K colors. In case that your screen is 6-bits, it will be capable to display up to 64 different colors using the most significant bits of the LCD controller lines, but you need to ensure that the additional control lines are also available in order to guarantee compatibility.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------