4GiB LPDDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4GiB LPDDR4

Jump to solution
1,649 Views
richardmarsh
Contributor I

We are looking to use a 1Gbx32 micron part (MT53D1024M32D4DT-046 WT:D) with an iMX8MM. 

As a trial we have swapped the LPDDR4 on an EVK SOM.

Is there a specific configuration file we would need in order to run the DDR tool (v310) to generate timing data and perform a stress test? Or can we use the mx8mm_micron_lpddr4_2gb_2d_1500m_200m_50m_32bit_1cs_RPAv15.ds file and just set the density to 4GB?

Cheers,

Richard

Labels (1)
0 Kudos
Reply
1 Solution
1,637 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi @richardmarsh,

 

For new memory part it is necessary to use RPA tool ( MX8M_Mini_LPDDR4_RPA_v16.xlsx ) available on:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

Also as you can see is a newer version so I recommend to update to this one.

 

Hope this helps you.

Regards,

Israel H.

View solution in original post

0 Kudos
Reply
1 Reply
1,638 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi @richardmarsh,

 

For new memory part it is necessary to use RPA tool ( MX8M_Mini_LPDDR4_RPA_v16.xlsx ) available on:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

Also as you can see is a newer version so I recommend to update to this one.

 

Hope this helps you.

Regards,

Israel H.

0 Kudos
Reply