4GB lpddr4 RAM working with iMX8MQ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

4GB lpddr4 RAM working with iMX8MQ

跳至解决方案
4,095 次查看
nirmalluhana
Contributor IV

Hi,

We going to design our custom board using iMX8MQ.

And we will use micron lpddr4 RAM which part number is "MT53D1024M32D4DT-053 AIT:D"

As I found one communication on the community at below link.

u-boot fails to boot with 4GB RAM on i.MX8mq 

So I just want to confirm there is any issue with 4GB lpddr4 RAM with the iMX8MQ processor? If possible, so can I use that part and able to use 4GB RAM?

Best,

Nirmal

标签 (1)
标记 (2)
1 解答
3,050 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

linux memory size is controlled by u-boot in i.MX8M software. One can try
attached u-boot patch. For new board recommended to follow Chapter 4 How to bring up a

new MX8M board MX8M_DDR_Tool_User_Guide document included in ddr test package.
i.MX8MSCALE DDR Tool Release 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,094 次查看
Liszt
Contributor V

It seem to not work on i.MX8M android 9.

What should we do on Android OS?

0 项奖励
回复
3,051 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

linux memory size is controlled by u-boot in i.MX8M software. One can try
attached u-boot patch. For new board recommended to follow Chapter 4 How to bring up a

new MX8M board MX8M_DDR_Tool_User_Guide document included in ddr test package.
i.MX8MSCALE DDR Tool Release 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------