4098x2160 resolution display support by i.MX8 QxP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

4098x2160 resolution display support by i.MX8 QxP

1,083件の閲覧回数
ajmalmali
Contributor II

Hi

A customer is trying to interface a 4096x2160 resolution hdmi display using the LVDS port of the iMX 8 QxP (through HDMI to LVDS converter).

I would like to ask you if i.MX 8QxP can support 4096x2160 display via LVDS. 

I understand that the iMx8Qm HDMI can support 4k displays.

Can you please confirm what is the maximum resolution supported by iMx8QxP LVDS?

 

Regards

Ajmal

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,064件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @ajmalmali,

I hope you are doing well.

One can refer to Section 15.3.1.2 Features of i.MXQXP Reference Manual.
LVDS interface supports display resolutions up to 1920x1080 (FHD) @ 60fps, 24bpp.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信