4 chips DDR3 and hybrid topology

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4 chips DDR3 and hybrid topology

1,033 Views
massimo2
Contributor III

Hello

I would like to improve my project.
If i have 4 x DDR3 chips on the same layer(top or bottom). From now i will call them "M" with a number.
May i crate an hybrid topology between T and fly-by using chip selects and multiple clocks?
Like
M1-M2 use CLK0 diff signal, CS0  data D[0-31]
&
M3-M4
use CLK1,CS1 and data D[32-63].
May i do that or i'm forced to use only first 32bits(data)?

The address lines could divide in 2 between 2 memory group like the T topology, like they are routed between M2 and M3 and then split.
  .--------------MPU----------.
 ck0            ||||addr       ck1
|M1||M2| <=====> |M3||M4|

2 Replies

996 Views
igorpadykov
NXP Employee
NXP Employee

Hi Massimo

>May i crate an hybrid topology between T and fly-by using chip selects and multiple clocks?

sorry this is not recommended.

>M3-M4 use CLK1,CS1 and data D[32-63].
>May i do that or i'm forced to use only first 32bits(data)?

MMDC allows only first 32bits(data) as described in

sect.44.12.1 MMDC Core Control Register (MMDCx_MDCTL) for "DSIZ" field

i.MX 6Dual/6Quad Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

996 Views
massimo2
Contributor III

Thank you.

0 Kudos
Reply