4 Channel 720P30 Video capture with single Soc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4 Channel 720P30 Video capture with single Soc

626 Views
shabbirlimdiwal
Contributor I

Hi,

For one of the upcoming products, we are looking for right architecture to implement SVM (Surround view monitoring) system. There will be 4 cameras mounted on car's front, rear, left and right side and we want to design a host system which can capture 4 channel Bayer/YUV data (each 720P@30), stitch them together to create one 720P view to be displayed on dashboard.

Can you suggest Freescale SoC which is able to capture 4 simultaneous channel 720P@30 fps?

If I am not wrong, one i.mx6 can capture two 720P30 channels at max. What if I want to capture 4 channels (I am fine using either CSI/paralle/both interfaces to achieve this use case).

If single SoC can't do that, what are the possible ways to achieve this use case?

Regards,
Shabbir

0 Kudos
1 Reply

269 Views
joanxie
NXP TechSupport
NXP TechSupport

for surround view, you can refer to the link as below:

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP

0 Kudos