4-5 second video lag while live streaming data through a wifi borescope in sabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4-5 second video lag while live streaming data through a wifi borescope in sabresd

1,569 Views
himanshugusain
Contributor III

Hi

I have few sabresd boards from freescale which runs on Android 4.4 & 5.0.2  

Recently I integrated the Wi-Fi Streaming application in all the tools

& found their is a lag of 4-5 in the data received in the Tool when connected to a borescope.

What could be possible issue , Is it something to do with the VPU in imx6 side

Regards

Himanshu

Labels (4)
0 Kudos
Reply
2 Replies

1,428 Views
igorpadykov
NXP Employee
NXP Employee

Hi Himanshu

had you tried to measure delays without wi-fi,

for vpu one can try to enable low-latency plugin as described in

RTSP gstreamer and vpudec 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,428 Views
himanshugusain
Contributor III

Igor

What do you mean by measure delay without wi-fi

You want me to store media file locally in tool & play from there

& compare that with a good known device.

Regards

Himanshu

0 Kudos
Reply