4.3 inch LCD parallel RGB interface support in i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4.3 inch LCD parallel RGB interface support in i.MX6

1,970 Views
amitjain
Contributor I

I am using i.MX6 processor with a 4.3 inch LCD parallel RGB interface with max clock frequency of 15MHz. We are using WinCE embedded compact 7 OS.Please let me know if i.MX6 can support this LCD.Someone told me that i.MX6 can only support LCD with clock frequency of 20MHZ or more.

Labels (1)
0 Kudos
4 Replies

609 Views
Yuri
NXP Employee
NXP Employee

  Below are considerations how to get 15 MHz of minimal value for  IPUx_HSP_CLK_ROOT;

IPUx_HSP_CLK_ROOT is reference clock for display / pixel clock. The display clock is (micro)programmable,

and its value may be less than  IPUx_HSP_CLK_ROOT. Theoretically it can achieve tens KHz.

Another thing, that the display frequency duty parameter may  be not 50%. 

According to the linked below Community thread :

" Referring to Figure 18-2, IPU1_HSP_CLK_ROOT may be selected to have 1 of 4 sources. These sources are highlighted in yellow on the northwest corner of the page and the previous paragraph states these are max values. Possible sources are 540, 528, 396, and 480 MHz. The 480 MHz is divided by 4 before the selector, so winds up being 120 MHz. Per the diagram, these are all divided by 2 for IPU1_HSP_CLK_ROOT. The result is 270, 264, 198, and 60 MHz choices". Note, really 120 MHz may be divided by 8 (please refer to CCM_CSCDR3 field descriptions

in the Reference Manual).

   So, 15 MHz is minimal value for  IPUx_HSP_CLK_ROOT. Next, we should consider parameter IP5 (Display interface clock period Tdicp) and IP6 (Display pixel clock period) in the i.MX6 Datasheets. Minumal period for display clock is defined by parameter DI_CLK_PERIOD, which is programmable.

Please refer to  section 37.4.10.3 (Timing generator) of the i.MX6 DQ Reference Manual. Display interface clock period is defined by 8-bit divider (interger part) ; this means minimal clock is ~60 KHz.

"Q&A: What are the maximum HSP_CLK frequency values?"

< https://community.freescale.com/docs/DOC-98282 >

Also, please take a look at Chapter 18 (Configuring the IPU Driver) of the "iMX6_Firmware_Guide.pdf"

in the Platfrom SDK package.

< https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null >

0 Kudos

609 Views
amitjain
Contributor I

Dear Yuri,

Thanks for your quick reply. This gives good insight on Display clock

period settings .

Can you please let me know that for LVDS based LCDs' what is the Display

interface clock frequency range?

Thanks and regards,

Amit Kumar Jain

Senior Lead Technical Architect

Competence Center India -- BNPO

Tel:911244598000

Mobile:919873719580

mailto:amit.jain@gi-de.com

Giesecke & Devrient India

Plot # 57,Sector 44,

Gurgaon--122003

http://www.gi-de.com

0 Kudos

609 Views
Yuri
NXP Employee
NXP Employee

From Table 9-6 (IP Parametric Table) in section 9.3.1 (LDB Overview)

of IMX6DQRM,Rev. 1, 04/2013 :

DI0_CLK, DI1_CLK- Display interface clock: 20-170 MHz

0 Kudos

609 Views
amitjain
Contributor I

Thanks Yuri.

Amit Kumar Jain

Senior Lead Technical Architect

Competence Center India -- BNPO

Tel:911244598000

Mobile:919873719580

mailto:amit.jain@gi-de.com

Giesecke & Devrient India

Plot # 57,Sector 44,

Gurgaon--122003

http://www.gi-de.com

0 Kudos