4路mipi加一路adv7180

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4路mipi加一路adv7180

Jump to solution
866 Views
强王
Contributor IV

目前imx6q 上面接了4路mipi和一路adv7180,分别使用都没有问题

需求:摄像头不会同时使用,但是会动态切换7180和mipi摄像头,驱动怎么修改

Message was edited by: Qiang Wang

0 Kudos
Reply
1 Solution
640 Views
igorpadykov
NXP Employee
NXP Employee

Hi Qiang

for switching between mipi and parallel camera one can use IOMUXC_GPR1

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
641 Views
igorpadykov
NXP Employee
NXP Employee

Hi Qiang

for switching between mipi and parallel camera one can use IOMUXC_GPR1

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply