32Khz output on CCM_CLKO2 pin of imx7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

32Khz output on CCM_CLKO2 pin of imx7

1,752件の閲覧回数
suryapradhan
Contributor II

Hello 

I need some info regarding generation of 32khz clk on CCM_CLKO2 of IMX7.

CCM_CLKO2 is connected to SD1_WP.

I am able to generate 24mhz but not 32khz.

Any suggestion.

Thanks & regards

Surya

ラベル(2)
0 件の賞賛
返信
1 返信

1,349件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi surya,

what error are you facing?

please take a look to this post which explains were the clock sources and dividers are. CCM_CLK02 follows same principle as SAIx_CLK_ROOT indicated here iMX7D : SAIx_CLK_ROOT minimum frequency value for SAI (Serial Audio Interface )module  


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信