Hi,
I'm using Yocto project environment for bring-up of freescale imx6 sabre Smard devices board. I see the kernel 3.10 is available.
But I need kernel 3.18 to be used from requirement perspective. Could you let me know how can do do that?
-ram
HI Ramprasad
one can look at
Freescale/linux-fslc at patches-3.18 · GitHub
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for for responding. I looked @ Freescale/linux-fslc at patches-3.18 · GitHub . But the current kernel I've for imx6 board was synced through git://git.freescale.com/imx/fsl-arm-yocto-bsp.git .
The link you provided says, patches-3.18 . But if I see there is no branch for 3.18, rather I see branches only for 3.10 and 3.14 kernel remaining are patches only. I looked @ Freescale/linux-fslc at patches-3.18 · GitHub and I selected the tab "branches" for viewing this. What is the difference? Is it a complete kernel or just a patch?
And how does it get plugged into yocto project environment? The earlier git I followed git://git.freescale.com/imx/fsl-arm-yocto-bsp.git looks like the one from freescale and the branch I used is under imx6. But the one you shared, how will I know whether it works for imx6 based boards?
Sorry if I'm asking some dumb questions. but I'm not familiar with these.
Hi,
Can someone help me on how to take this forward?