2GB RAM is used for Android 9 booting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2GB RAM is used for Android 9 booting

Jump to solution
769 Views
vinothkumars
Senior Contributor IV

Hi All,

I have only 2GB RAM in my IMX8QM Custom Board (IMX8QM MEK have 6GB RAM).
But, my system image size is morethan 1GB. I want to know, is it enough for booting Android 9.

Memory configuration in uboot,
  1. sdram 1 size - 1GB
  2. sdram 2 size - 1GB
  3, Number of Banks - 8

with this configuration I got iomap kernel hang.


I need some work around for 2GB RAM.

 

Regards,
Vinothkumar Sekar
0 Kudos
1 Solution
756 Views
BiyongSUN
NXP Employee
NXP Employee

I think you need to create very basic computer concept.

The image size is not the size for the memory. 

How many memory size needed depends on the use case. How many applications will be used. 

The system image is rootfs. will not be entirely load to the memory. 

It likes you have 2T hard disk for your x86/x64 compute and you have 32G memory. 

and your concept is if I want to use this 2T disk computer, I need 2T memory as well. 

View solution in original post

0 Kudos
2 Replies
757 Views
BiyongSUN
NXP Employee
NXP Employee

I think you need to create very basic computer concept.

The image size is not the size for the memory. 

How many memory size needed depends on the use case. How many applications will be used. 

The system image is rootfs. will not be entirely load to the memory. 

It likes you have 2T hard disk for your x86/x64 compute and you have 32G memory. 

and your concept is if I want to use this 2T disk computer, I need 2T memory as well. 

0 Kudos
746 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good