Hi All,
We're using i.MX6 sololite EVK (android N7.1.1_1.0.0-ga) as our development platform, now we want to make our board and change the 1GB LPDDR2 to 2GB LPDDR2 (or DDR3) as well as the eMMC from 8GB to 16GB. my question is that is it possible for us to use the mfg tool on the new board, if not, is there any source/patch available for that? thanks.
B.R.
Sun
Hi Sun
please find new calibration coefficients for new board running ddr test
i.MX6/7 DDR Stress Test Tool V2.70
put them to uboot/board/freescale/mx6slevk/imximage.cfg
and rebuild image. To use mfg tool on the new board
rebuild its firmware (files in firmware folder) using sect.6.2 Manufacturing
Tool, MFGTool attached Yocto Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------