256Mx16 4Gb DDR3 SDRAM one bank?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

256Mx16 4Gb DDR3 SDRAM one bank?

Jump to solution
1,036 Views
hermanzeilstra
Contributor I

Hello,

Stupid question, can I make an I.MX7 work with one bank of 256Mx16 4Gb DDR3 SDRAM or do I need two banks to connect all data pins on the chip?

ddr3.jpg

Data Strobe: output with read data, input with write data. Edge-aligned with read data, centered in write data. For the x16, DQSL corresponds to the data on DQL0-DQL7; DQSU corresponds to the data on DQU0-DQU7. The data strobes DQS, DQSL, and DQSU are paired with differential signals DQS#, DQSL#, and DQSU#, respectively, to provide differential pair signaling to the system during reads and writes. DDR3 SDRAM supports differential data strobe only and does not support single-ended.

Can I connect DQL0-DQL7 to ADDR0-7 and DQU0-DQU7 to to ADDR8-15 ? 

And then conect the differential signals of the datastrobes DQS, DQSL, and DQSU & DQS#, DQSL#, and DQSU#

Thanks

Herman

Labels (1)
0 Kudos
1 Solution
829 Views
igorpadykov
NXP Employee
NXP Employee

Hi Herman

i.MX7D supports memory data width 16.

Best regards
igor

View solution in original post

3 Replies
829 Views
igorpadykov
NXP Employee
NXP Employee

Hi Herman

please check sect.3.4. DDR Connection information

Hardware Development Guide for i.MX7Dual and 7Solo Applications Processors
http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf

and ddr connections on Sabre SD schematic, it is composed from two x16 ddr chips

Schematics (2)
Design files for i.MX 7Dual (REV D)
Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual (REV D)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
829 Views
hermanzeilstra
Contributor I

Hello Igor,

Thank you very much for responding.

I was wondering, should a design work with only two Byte Groups connected.

Thanks

Herman

0 Kudos
830 Views
igorpadykov
NXP Employee
NXP Employee

Hi Herman

i.MX7D supports memory data width 16.

Best regards
igor