1PPS pin on iMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1PPS pin on iMX8MP

Jump to solution
1,577 Views
khang_letruong
Senior Contributor III

Dear NXP Team,

I would like to connect the PPS output of GNSS module to iMX8MP but I wonder if it should be a generic GPIO or a specific GPIO like in the following discussion : https://community.nxp.com/t5/i-MX-Processors/how-to-config-1PPS-on-imx8qxp/m-p/1050249

We plan to use the below :

+       pinctrl_gnsspps: gnsspps_grp {
+               fsl,pins = <
+                       MX8MP_IOMUXC_SAI3_RXD__GPIO4_IO30       0x19
+               >;
+       };

 

Is our configuration correct ?

 

Best Regards,

Khang

 

0 Kudos
Reply
1 Solution
1,534 Views
khang_letruong
Senior Contributor III
0 Kudos
Reply
3 Replies
1,535 Views
khang_letruong
Senior Contributor III
0 Kudos
Reply
1,570 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
1,563 Views
khang_letruong
Senior Contributor III

Hi @joanxie ,

Thanks for the link but it seems that I was not clear in my use-case : I would like to capture the 1PPS input signal from a GPS/GNSS module rather than to generate the 1PPS output signal.

I found the similar use-case : https://community.nxp.com/t5/i-MX-Processors/i-MX6s-dl-input-PPS-to-FEC-for-PTP-Grand-master-ENET-15...

or this : https://community.nxp.com/t5/i-MX-Processors/Ntpd-gpsd-GPS-PPS/m-p/773608

Best Regards,

Khang

 

0 Kudos
Reply