1920x1200 support on iMX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1920x1200 support on iMX6Q

922 Views
jorisguisson
Contributor I

I'm evaluating the iMX6Q to see if it fits our needs. One of them being the need for supporting 1920x1200 on the HDMI output. It doesn't out of the box, but after some searching on this board it seems that you can add your own resolutions to ./drivers/video/mxc/mxc_edid.c. But is this going to work ? Or is there some kind of hardware limitation which will make this not work ?

Labels (1)
0 Kudos
1 Reply

605 Views
SergioSolis
NXP Employee
NXP Employee

You are correct, you can set your own resolution and yes, it does support 1920x1200 on the HDMI output.

0 Kudos