Imx6 continuous playback test found sometimes unable to play all the video will be stuck in black

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

  Imx6 continuous playback test found sometimes unable to play all the video will be stuck in black

563 Views
fdact
Contributor I

Hi,

     I got the video play problem on imx6 sabresd_6dq  with android 4.2.2 and kernel .

     Continuous playback test found sometimes unable to play all the video will be stuck in black.

     The below is a part of crash logcat, more log please reference the attachment :

     

I/OMXPlayer( 2238): Seek to 909000
I/OMXPlayer( 2238): LEVEL: 1 FUNCTION: FlushComponent LINE: 944
I/OMXPlayer( 2238): Surface::dequeueBuffer returned error -16
I/OMXPlayer( 2238): Seek to 12733000
I/OMXPlayer( 2238): LEVEL: 1 FUNCTION: FlushComponent LINE: 944
I/OMXPlayer( 2238): Surface::dequeueBuffer returned error -16
I/OMXPlayer( 2238): Seek to 12733000
I/OMXPlayer( 2238): LEVEL: 1 FUNCTION: FlushComponent LINE: 944
I/OMXPlayer( 2238): Surface::dequeueBuffer returned error -16
I/OMXPlayer( 2238): Seek to 73670000
I/OMXPlayer( 2238): LEVEL: 1 FUNCTION: FlushComponent LINE: 944
I/OMXPlayer( 2238): Surface::dequeueBuffer returned error -16
I/OMXPlayer( 2238): Seek to 76398000
I/OMXPlayer( 2238): LEVEL: 1 FUNCTION: FlushComponent LINE: 944
I/OMXPlayer( 2238): Surface::dequeueBuffer returned error -16

 

 

Thanks.

Original Attachment has been moved to: android_video.log.zip

Labels (3)
Tags (1)
0 Kudos
2 Replies

404 Views
igorpadykov
NXP Employee
NXP Employee

Hi ferdinand

L3.0.35 kernel has issues with memory leak as answered by experts on

Long running vpu task with memory leak bug on imx6 | NXP Community 

recommended to migrate to more new kernels, where this was fixed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

404 Views
fdact
Contributor I

But I didn't find any Vpu memory related log in the kernel to print out when the problem occurs.

And the log print out a lot of "dequeueBuffer: can't dequeue multiple buffers without setting the buffer count".

I'm not sure if the two are related?

0 Kudos