10BaseT not working on iMX53 platfrom running WEC7.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

10BaseT not working on iMX53 platfrom running WEC7.

939 Views
muzammalahmed
Contributor I

Hi all,

I'm trying to make 10Base-T work on a platform running WEC7 on iMX53. The Phy being used is LAN8720. 100Base-T works fine. Anyone run into this issue? Please help.

- Muzammal Ahmed

Labels (2)
0 Kudos
Reply
2 Replies

813 Views
fear_nada
Contributor II

same issue here WINCE6 i.mx28 + lan8720. Why "10 Base-T" not supported in Adeneo BSP ? Can any one try check 10mbit + Linux BSP?

0 Kudos
Reply

813 Views
fear_nada
Contributor II

we need detect Speed and Duplex at ENETEnetInit()

like in this sample code:

  
Sleep(200);
RegValue =  MII_READ_COMMAND(MII_LAN87xx_SCSR);
   RegValue |= BF_ENET_MAC_MMFR_PA(index);
   HW_ENET_MAC_MMFR_WR(MAC0,RegValue);
   Sleep(200);
MIIReg = HW_ENET_MAC_MMFR_RD(MAC0);
RETAILMSG(1, (TEXT("ENET: index = %d  RegValue = %x MII_LAN87xx_SCSR MIIReg= %x \r\n"),index,RegValue,MIIReg));

  

if(MIIReg & (0x1000))
{

    DEBUGMSG(ZONE_FUNCTION, (TEXT("ENET: STATUS: Auto-Negotiation complite at init \r\n")));

    }

  

HcdSpeed=(((UINT16)MIIReg & 0x001C)>>2);
if(1==HcdSpeed)
{

    BW_ENET_MAC_RCR_RMII_10T(index, 1); // eai set 10-Base T  Enables 10Mbps mode of the RMII.

    BW_ENET_MAC_RCR_DRT(index, 1);    //eai Disable reception of frames while transmitting (normally used for half duplex mode)

    BW_ENET_MAC_TCR_FEDN(index,0);    //eai full duplex disabled

DEBUGMSG(ZONE_FUNCTION, (TEXT("PHY_STAT_10HDX at init \r\n")));

}
else if(5==HcdSpeed)

{

    BW_ENET_MAC_RCR_RMII_10T(index, 1); // eai set 10-Base T  Enables 10Mbps mode of the RMII.

    BW_ENET_MAC_RCR_DRT(index, 0);    //eai en reception of frames while transmitting

    BW_ENET_MAC_TCR_FEDN(index,1);    //eai full duplex en

DEBUGMSG(ZONE_FUNCTION, (TEXT("PHY_STAT_10FDX  at init \r\n")));

}

else if(2==HcdSpeed)
{

    BW_ENET_MAC_RCR_RMII_10T(index, 0); // eai set 100-Base T

    BW_ENET_MAC_RCR_DRT(index, 1);    //eai Disable reception of frames while transmitting (normally used for half duplex mode)

    BW_ENET_MAC_TCR_FEDN(index,0);    //eai full duplex disabled

DEBUGMSG(ZONE_FUNCTION, (TEXT("PHY_STAT_100HDX at init \r\n")));

}

else if(6==HcdSpeed)
{

  

    BW_ENET_MAC_RCR_RMII_10T(index, 0); // eai set 100-Base T  Enables 10Mbps mode of the RMII.

    BW_ENET_MAC_RCR_DRT(index, 0);    //eai en reception of frames while transmitting

    BW_ENET_MAC_TCR_FEDN(index,1);    //eai full duplex en

DEBUGMSG(ZONE_FUNCTION, (TEXT("PHY_STAT_100FDX  at init \r\n")));

  

}
0 Kudos
Reply