1080p 30fps * 4ch input availability in i.MX6 via ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1080p 30fps * 4ch input availability in i.MX6 via ethernet

Jump to solution
1,396 Views
JHY
Contributor IV

I found i.MX6 can support  up to 720p 4ch cameras.

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP

If there are 1080p 30fps 4ch cameras, is it possible to capture image data using SABRE2-AI board and AVB?

Best regards.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,131 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I am afraid the configuration of 4 channels 1080p 30 fps cannot be

processed via Ethernet of i.MX6 because of performance lack, since
~237 Mbytes /sec throughput is required for raw data. If encode the
images, VPU has no enough performance for it too.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,132 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I am afraid the configuration of 4 channels 1080p 30 fps cannot be

processed via Ethernet of i.MX6 because of performance lack, since
~237 Mbytes /sec throughput is required for raw data. If encode the
images, VPU has no enough performance for it too.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply