【1】How to connect the AUDMUX port with a voice codec and the PCM port of Bluetooth simultaneously?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

【1】How to connect the AUDMUX port with a voice codec and the PCM port of Bluetooth simultaneously?

1,159 Views
johnphy
Contributor I

Hi,

     We are using I.MX6Q, and we connect the AUDMUX  port  with the  voice codec chip  WM8962B. Now we also need  to use the PCM audio function of  the bluetooth module. So can anybody help to give some advice? Can we connect the AUDMUX  port with a voice codec and the PCM port of Bluetooth simultaneously?

    Thanks a lot!

0 Kudos
Reply
1 Reply

912 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Would you be nice enough to share the part number of the devices you want to connect?

Regards,

Alejandro

0 Kudos
Reply