更新4.1.15内核不成功

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

更新4.1.15内核不成功

Jump to solution
1,119 Views
小辉哥
Contributor III

我想把imx6ul的内核版本更新为4.1.15,我执行 repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga命令后,出现:

fatal: read error: Connection reset by peer

fatal: cannot obtain manifest git://git.freescale.com/imx/fsl-arm-yocto-bsp.git

是什么原因导致的,我之前使用repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.38-6UL_ga是可以的,现在都执行不成功了,我该怎么办,需要你们的帮助,谢谢。

Labels (4)
0 Kudos
Reply
1 Solution
740 Views
gary_bisson
Senior Contributor III

Hi,

Yes as said in this post, the server seems to be down:

git clone error

Is there a maintenance operation going on? How long will it be?

NXP, please advise.

Regards,

Gary

View solution in original post

0 Kudos
Reply
2 Replies
741 Views
gary_bisson
Senior Contributor III

Hi,

Yes as said in this post, the server seems to be down:

git clone error

Is there a maintenance operation going on? How long will it be?

NXP, please advise.

Regards,

Gary

0 Kudos
Reply
740 Views
小辉哥
Contributor III

恩 最近可以更新代码了,谢谢!

0 Kudos
Reply