[INFO] | Product Info: i.MX6Q/D/S |
[INFO] | VPU firmware version: 2.3.10_r40778 |
[INFO] | VPU library version: 5.4.16 |
[INFO] | Format: STD_MPEG4 |
[INFO] | MPEG4 class: MPEG4 |
[INFO] | Output file "enc.m4v" opened. |
[INFO] | Product Info: i.MX6Q/D/S |
[INFO] | VPU firmware version: 2.3.10_r40778 |
[INFO] | VPU library version: 5.4.16 |
[INFO] | Capture/Encode fps will be 30 |
[INFO] | chromaInterleave 1, mapType 0, linear2TiledEnable 0 |
ov3640_write_reg:write reg error:reg=3012,val=80
[INFO] | sensor chip is ov5640_camera |
Not support the resolution in camera
麻烦大师帮我看看,应该怎么解决。
for your new camera, did you build in the bsp? if not, pls build this camera in the bsp first
did you use ov3640?
pls try to use two commands before use unit test
"
modprobe mxc_v4l_capture
modprobe ov3640_camera
"
你好,我使用的是usb摄像头。