怎样在UBOOT中给EMMC分区

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

怎样在UBOOT中给EMMC分区

Jump to solution
6,043 Views
强王
Contributor IV

怎样在UBOOT中给EMMC分区

Labels (2)
0 Kudos
Reply
1 Solution
4,012 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Qiang,

Are you using the BSP provided by freescale? In the i.MX_6_SABRE-SD_Linux_User's_Guide.pdf document, you can see details on 6.2 Download Images by U-Boot. Take the BSP  L3.10.17_1.0.0 as an example, you can refer to  the attachment file.

Hope this can help you. Any questions you can contact me easily.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

8 Replies
4,013 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Qiang Wang,

What platform and which version of BSP are you using?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,013 Views
强王
Contributor IV

yocto imx6qsabresd uboot(2014.02)

0 Kudos
Reply
4,013 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Qiang,

Are you using the BSP provided by freescale? In the i.MX_6_SABRE-SD_Linux_User's_Guide.pdf document, you can see details on 6.2 Download Images by U-Boot. Take the BSP  L3.10.17_1.0.0 as an example, you can refer to  the attachment file.

Hope this can help you. Any questions you can contact me easily.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,013 Views
强王
Contributor IV

Dear Dan:

     我的问题是:

     假如EMMC没有分区,我想在UBOOT中给EMMC分2个分区

     6.2讲的是EMMC启动以及在内核中分区

0 Kudos
Reply
4,013 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Qiang,

Have you solved your questions, if yes please help click the Correct Answer button, thank you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,013 Views
强王
Contributor IV

Dear Dan:

     谢谢你的及时回复,看来只能自己移植命令进去了!!!

0 Kudos
Reply
4,013 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Qiang,

不客气的:smileyhappy:,欢迎有问题继续在本论坛中创建提问哈~~

Have a nice day

Best Regards

Dan

0 Kudos
Reply
4,013 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Qiang,

是要在内核启动以后,分区的命令才可以使用,我刚跟别的同事确认了一下,在u-boot中对EMMC分区的话是不可以的,没有命令可以使用。不过这是针对2012以及以前的版本,新版本2014版本的u-boot我们这边不是很清楚。

这里还是建议你使用NFS启动,或者是我上述给你的方法,对EMMC分区。希望对你有帮助。
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------