NXP有没有一款SAM芯片可以支持在Android 6.0上应用,NXP可以给出相关应用资料。
Hi,
Could you tell me which chip and board are you using?
Have a nice day
Rita
你好!
我们的cpu 是mtk6737 我们本来想用pn7462完成NFC和管理SAM的,但是没有找到pn7462在Android系统的相关资料。现在我们想着用pn7150实现nfc的功能,SAM用其他芯片。你能给我们一个更好的方案吗?
期待你的答复
13102370205@163.com
发件人: b45499
发送时间: 2017-05-05 13:45
收件人: 小雨 李
主题: Re: - Re: 寻求一款PSAM芯片,能够应用于Android 6.0
NXP Community
Re: 寻求一款PSAM芯片,能够应用于Android 6.0
reply from Rita Wang in i.MX Community - View the full discussion
Hi,
Could you tell me which chip and board are you using?
Have a nice day
Rita
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in i.MX Community by email or at NXP Community
Following Re: 寻求一款PSAM芯片,能够应用于Android 6.0 in these streams: Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences