我有一块客户的MX6-SabreSD开发板,没有RGB接口。而客户打算使用RGB接口的4英寸屏(分辨率为480*800),所以打算使用LVDS转RGB的转接板。
屏的手册中的DPI Interface Timing如下:
目前,ldb.c内各参数如下:
但是显示是花屏,颜色也不对
有人用过类似转换板吗?屏的手册提供的各参数是针对RGB接口的,那ldb.c中应该如何设置 fb_videomode各参数呢?
Which version of BSP are you using?
是android4.2.2的bsp
Is the screen work well?
Hi,
You can refer to the thread Porting LVDS LCD With Low Resolution to i.MX6 .
And the follow documents:
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------