hi,
我尝试使用imx6D的SPI5(master)与SPI转UART(slave)进行通信,slave设备要求CS保持两个字节有效(cmd+data),但是imx6每发送一个字节,CS就会被拉高,在该情况下我的设备就无法获取data,使用spidev_test.c设置cs_change不起作用,查看spi-imx.c驱动似乎没有对cs_change进行任何处理,根据数据手册IMX6DQRM第21章的描述, 我想设置成Figure 21-8 的状态,当我设置SS_CTL[3:0] 0000 时,内核好像被hangs up了,当设置SS_CTL[3:0]为SS_CTL[3:0] 0001时,CS输出状态为Figure 21-9,kernel为3.14.52,对此不知道该如何去设置,还请不吝指教。
谢谢!
Alee
Solved! Go to Solution.
FYI. linux-imx.git - i.MX Linux Kernel
For example:
&ecspi1 {
fsl,spi-num-chipselects = <1>;
cs-gpios = <&gpio4 9 0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi1>;
status = "okay";
flash: m25p80@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "st,m25p32";
spi-max-frequency = <20000000>;
reg = <0>;
};
pinctrl_ecspi1: ecspi1grp {
fsl,pins = <
MX6QDL_PAD_KEY_COL1__ECSPI1_MISO 0x100b1
MX6QDL_PAD_KEY_ROW0__ECSPI1_MOSI 0x100b1
MX6QDL_PAD_KEY_COL0__ECSPI1_SCLK 0x100b1
MX6QDL_PAD_KEY_ROW1__GPIO4_IO09 0x1b0b0
>;
};
you can change the CS to GPIO. Then you can use the GPIO to output the CS signal that you need.
hi jim,
thank you for the answer,I also think about it ,but it is complex ,because it seem like I can't use the spi controller with no CS pin.I'm try to give it another CS pin, but all of the SPI5 CS pin used by other functions,so what should I do if I change the CS to GPIO.
Thanks,
Alee
FYI. linux-imx.git - i.MX Linux Kernel
For example:
&ecspi1 {
fsl,spi-num-chipselects = <1>;
cs-gpios = <&gpio4 9 0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi1>;
status = "okay";
flash: m25p80@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "st,m25p32";
spi-max-frequency = <20000000>;
reg = <0>;
};
pinctrl_ecspi1: ecspi1grp {
fsl,pins = <
MX6QDL_PAD_KEY_COL1__ECSPI1_MISO 0x100b1
MX6QDL_PAD_KEY_ROW0__ECSPI1_MOSI 0x100b1
MX6QDL_PAD_KEY_COL0__ECSPI1_SCLK 0x100b1
MX6QDL_PAD_KEY_ROW1__GPIO4_IO09 0x1b0b0
>;
};
hi, jim
Thanks for your help.
it's work
thanks!!!
you are welcome