关于i.MX8MQ中HDMI和MIPI双显的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于i.MX8MQ中HDMI和MIPI双显的问题

6,052 Views
晓锋潘
Contributor I

我在imx8mq android 8.1.0_1.3.0中需要支持HDMI和MIPI双显,分辨率皆为1080p,但mipi显示屏无显示,MIPI显示屏使用DCSS作为输入源的时候显示是OK的。我的双显的dts文件参见附件,板子启动log信息见附件。

log信息部分显示如下:

yx8210hvcn_8mq:/ # dmesg |grep drm

[    1.582980] [drm] Initialized

[    1.595165] nwl_dsi-imx mipi_dsi@30A00000: Added drm bridge!

[    1.603134] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

[    1.609827] [drm] No driver support for vblank timestamp query.

[    1.615883] imx-drm display-subsystem: bound imx-dcss-crtc.0 (ops dcss_crtc_ops)

[    1.651142] [drm] hdmi-audio-codec driver bound to HDMI

[    1.656392] imx-drm display-subsystem: bound 32c00000.hdmi (ops imx_hdp_imx_ops)

[    1.663898] imx-drm display-subsystem: No connectors reported connected with modes

[    1.671487] [drm] Cannot find any crtc or sizes - going 1024x768

[    1.707739] imx-drm display-subsystem: fb0:  frame buffer device

从红色部分来看,似乎是因为没找到crtc,请帮我看一下,谢谢!

另:屏的时序设置在屏的驱动文件中,具体如下:

static const struct display_timing startek_default_timing = {
 .pixelclock = { 66000000, 120000000, 132000000 },
 .hactive = { 1080, 1080, 1080 },
 .hfront_porch = { 20, 20, 20 },
 .hsync_len = { 2, 2, 2 },
 .hback_porch = { 34, 34, 34 },
 .vactive = { 1920, 1920, 1920 },
 .vfront_porch = { 10, 10, 10 },
 .vsync_len = { 2, 2, 2 },
 .vback_porch = { 4, 4, 4 },
 .flags = DISPLAY_FLAGS_HSYNC_LOW |
   DISPLAY_FLAGS_VSYNC_LOW |
   DISPLAY_FLAGS_DE_LOW |
   DISPLAY_FLAGS_PIXDATA_NEGEDGE,
};

Labels (1)
0 Kudos
2 Replies

3,977 Views
weiping_liu
NXP Employee
NXP Employee

1. there is no mode specified by the panel.

I can see this error in log:

[    2.377857] /mipi_dsi_bridge@30A00000/panel@0: could not find display-timings node

[    2.385442] /mipi_dsi_bridge@30A00000/panel@0: no timings specified

 

2. according to the driver, it should use the timings hard-coded in driver. Still, the LCDIF does not receive any mode:

[    2.512500] mxsfb_drm 30320000.lcdif: No connectors reported connected with modes

 

3.  there is a problem with HDMI too, because there is no CRTC to specify a mode:

[ 2.520060] [drm] Cannot find any crtc or sizes - going 1024x768

 

In order to get more information about this, please enable DRM debug (use drm.debug=0x1F in cmdline when booting the kernel). Then run dmesg and send us the whole dump of dmesg output.

 

0 Kudos

3,977 Views
lingguan
Contributor II

My error is:

[ 3.624105] [drm:drm_calc_timestamping_constants] crtc 33: hwmode: htotal 2432, vtotal 1099, vdisplay 1080
[ 3.624112] [drm:drm_calc_timestamping_constants] crtc 33: clock 80192 kHz framedur 33329608 linedur 30327
[ 3.624119] [drm:drm_atomic_helper_commit_modeset_disables] modeset on [ENCODER:45:TMDS-45]
[ 3.624123] [drm] Link rate is too high - forcing link to lower rate
[ 5.123379] [drm:hdmi_phy_init_t28hpc] *ERROR* HDMI mailbox access failed
[ 5.123384] [drm:imx_hdp_mode_setup] *ERROR* Failed to initialise HDP PHY

How to solve this problem?

Sincerely.

0 Kudos