关于IMX6的SD卡的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于IMX6的SD卡的问题

1,672 Views
zhangkang90125
Contributor I

在IMX6的数据手册中发该芯片的SDIO接口支持SDXC这个标准,请问是否可以确认IMX6是支持512GB的SD卡??

The IMX6's SDIO interface supports SDXC.Can you confirm IMX6 support capacity of 512GB SD card?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,005 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

According with section 27.2 "Driver Features" of the i.MX6 Linux Reference Manual (attached):

"The MMC driver supports the following features:

..• SD3.0 cards."

Also, information on link below may be useful:

Secure Digital - Wikipedia, the free encyclopedia

So, the card support is not dependent of the card capacity. If the card is v3.0 (SDXC UHS-I) it should be supported. If the card is v4.0 (SDXC UHS-II) it should be supported in SDXC UHS-I mode.

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply