在imx6q 平台上使用下: ./mxc_vpu_test.out -D "-i /opt/test.264 -f 2 -w 720 -h 480-j 0 -k 0 -x 16" 可以显示视频,但是屏幕非常闪烁,还有竖着的纹路。 但是使用 ./mxc_vpu_test.out -D "-i /opt/test.264 -f 2 -w 720 -h 480-j 0 -k 0 -x 17" 时, 视屏显示正常, 这是什么问题呢?
The kernel image is build by myself. and there are some configs will led this issue? could you give me some suggest? thank you!
what bsp version do you use? did you change anything on your board? x17 is overlay of x16, pls try to use command:
cat /sys/class/video4linux/video17/name and cat /sys/class/video4linux/video16/name, what do you get?
thks for you answer
bsp is 3.0.35, follow is the result the the two command:
cat /sys/class/video4linux/video17/name
DISP3 FG
~ # cat /sys/class/video4linux/video16/name
DISP3 BG
did you use demo image or image build by yourself, what source code do you change? I can play the video on the video16 and video 17 successfully,