使用的IMX6Duallite平台, 老化3天后出现黑屏现象(LVDS屏的数据线无波形),LOG提示timeout when waiting for flip irq。

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

使用的IMX6Duallite平台, 老化3天后出现黑屏现象(LVDS屏的数据线无波形),LOG提示timeout when waiting for flip irq。

2,118 Views
rober12609
Contributor I

分析:
1 示波器测试LVDS_T0+/T0-,LVDS_T1+/T1-,LVDS_T2+/T2-,LVDS_T3+/T3- 数据信号无任何的波形,只有偏置直流电平,但测试LVDS_CLK+/CLK-信号幅度正常,频率65MHZ正常
2 软件分析LOG提示:timeout when waiting for flip irq,显示irq异常而返回。LOG见附件
   (1)   软件加入:write /sys/module/galcore/parameters/gpu3DMinClock 3 待测试。

   (2)看贵司论坛的补丁如下的修改是否适应改IC?修改也没什么效果 。

- imx6q_set_lpm(WAIT_UNCLOCKED);
+ //imx6q_set_lpm(WAIT_UNCLOCKED);
cpu_do_idle();
- imx6q_set_lpm(WAIT_CLOCKED);
+ //imx6q_set_lpm(WAIT_CLOCKED);
spin_unlock(&master_lock);
goto done;

(2 ) 看代码是ipu出了问题,ipu_pre_yres_is_small。查询网上有一些客户提出该问题给NXP,但没得到正面解决问题的补丁。如帖子(Re: mxc_sdc_fb fb.16: timeout when waiting for fli... - NXP Community)
max_lu
Contributor I

Hi,

Thanks to NXP's support team, this issue is solved. Please follow https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf. And this fix also been included in NXP's kernel
 https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.

0 Kudos
Reply
13 Replies

2,087 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which board are you using?

Which BSP are you using?

0 Kudos
Reply

2,084 Views
rober12609
Contributor I

android5.1

bsp linux 3.14.52

 

0 Kudos
Reply

2,071 Views
rober12609
Contributor I

IMX6Duallite

0 Kudos
Reply

2,074 Views
rober12609
Contributor I

IMX6 Duallite

Tags (1)
0 Kudos
Reply

2,068 Views
rober12609
Contributor I

IC screen printed as MCIMX6U7CVM08AC

0 Kudos
Reply

2,031 Views
rober12609
Contributor I

I have referred to this blog post before, but it cannot solve our problem

0 Kudos
Reply

2,019 Views
rober12609
Contributor I

Looking at the blog below, there were issues with handling them, but we couldn't find any relevant patches (https://source.codeaurora.org/external/imx/linux-imx

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

Thanks to NXP's support team, this issue is solved. Please follow https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf. And this fix also been included in NXP's kernel
 https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

 

 

 

 

0 Kudos
Reply

1,932 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,023 Views
jimmychan
NXP TechSupport
NXP TechSupport

Have you try the newer version of BSP?

0 Kudos
Reply

2,018 Views
rober12609
Contributor I

Looking at the blog below, there were issues with handling them, but we couldn't find any relevant patches (https://source.codeaurora.org/external/imx/linux-imx

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

Thanks to NXP's support team, this issue is solved. Please follow https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf. And this fix also been included in NXP's kernel
 https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

0 Kudos
Reply

2,012 Views
rober12609
Contributor I

论坛:https://community.nxp.com/t5/i-MX-Processors/mxc-sdc-fb-fb-16-timeout-when-waiting-for-flip-irq/m-p/...

NXP's kernel https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

rober12609_1-1699586455670.png

 

max_lu
Contributor I
 

Hi,

 

Thanks to NXP's support team, this issue is solved. Please follow https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf. And this fix also been included in NXP's kernel https://source.codeaurora.org/external/imx/linux-imx, branch imx_3.14.52_1.1.0_ga, commit id bbb48bbc88284f29c6980ee70373f91c7c86ff42 and 3f575c4967001c239634565c1327f4cc1a30b2c4.

 

0 Kudos
Reply

1,886 Views
rober12609
Contributor I

IC screen printed as MCIMX6U7CVM08AC  。Which model does this IC belong to in the following list?

BSP already has the following patches by default, but the problem still exists.

patch:(if (cpu_is_imx6q() && imx_get_soc_revision() == IMX_CHIP_REVISION_2_0) {)

static inline bool cpu_is_imx6sl(void) { return __mxc_cpu_type == MXC_CPU_IMX6SL; }
static inline bool cpu_is_imx6dl(void) { return __mxc_cpu_type == MXC_CPU_IMX6DL; }
static inline bool cpu_is_imx6sx(void) { return __mxc_cpu_type == MXC_CPU_IMX6SX; }
static inline bool cpu_is_imx6ul(void) { return __mxc_cpu_type == MXC_CPU_IMX6UL; }
static inline bool cpu_is_imx6q(void) { return __mxc_cpu_type == MXC_CPU_IMX6Q; }

 

if (cpu_is_imx6q() && imx_get_soc_revision() == IMX_CHIP_REVISION_2_0) {
clk[IMX6QDL_CLK_LDB_DI0_SEL] = imx_clk_mux_flags("ldb_di0_sel", base + 0x2c, 9, 3, ldb_di_sels, ARRAY_SIZE(ldb_di_sels), CLK_SET_RATE_PARENT);
clk[IMX6QDL_CLK_LDB_DI1_SEL] = imx_clk_mux_flags("ldb_di1_sel", base + 0x2c, 12, 3, ldb_di_sels, ARRAY_SIZE(ldb_di_sels), CLK_SET_RATE_PARENT);
} else {
/*
* The LDB_DI0/1_SEL muxes are registered read-only due to a hardware
* bug. Set the muxes to the requested values before registering the
* ldb_di_sel clocks.
*/
disable_anatop_clocks();
init_ldb_clks(np);
clk[IMX6QDL_CLK_LDB_DI0_SEL] = imx_clk_mux_ldb("ldb_di0_sel", base + 0x2c, 9, 3, ldb_di_sels, ARRAY_SIZE(ldb_di_sels));
clk[IMX6QDL_CLK_LDB_DI1_SEL] = imx_clk_mux_ldb("ldb_di1_sel", base + 0x2c, 12, 3, ldb_di_sels, ARRAY_SIZE(ldb_di_sels));
}

 

 

 

 

0 Kudos
Reply