你好!如果我想用i.mx6UL自带的SPI1挂两个SPI设备,其中一个设备的片选是SPI1_SS0,另外一个设备的片选用普通GPIO模拟,可以实现么?非常感谢!

cancel
Showing results for 
Search instead for 
Did you mean: 

你好!如果我想用i.mx6UL自带的SPI1挂两个SPI设备,其中一个设备的片选是SPI1_SS0,另外一个设备的片选用普通GPIO模拟,可以实现么?非常感谢!

Jump to solution
574 Views
怡帆华
Contributor I

你好!如果我想用i.mx6UL自带的SPI1挂两个SPI设备,其中一个设备的片选是SPI1_SS0,另外一个设备的片选用普通GPIO模拟,可以实现么?非常感谢!

Labels (1)
0 Kudos
1 Solution
258 Views
jimmychan
NXP TechSupport
NXP TechSupport

You can use gpio for both chip select signals. Here is the example:

https://community.nxp.com/message/1023960?commentID=1023960#comment-1023960 

View solution in original post

0 Kudos
1 Reply
259 Views
jimmychan
NXP TechSupport
NXP TechSupport

You can use gpio for both chip select signals. Here is the example:

https://community.nxp.com/message/1023960?commentID=1023960#comment-1023960 

0 Kudos