三屏显示时HDMI不是设置为1920x1080吗?怎么变成240x320?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

三屏显示时HDMI不是设置为1920x1080吗?怎么变成240x320?

2,942 Views
wumr
Contributor I

基于imx6q的3.14.28的BSP,实现LVDS+LVDS+HDMI三屏显示
1.uboot参数
setenv bootargs console=ttymxc0,115200 video=mxcfb0:dev=ldb,LDB-XGA,if=RGB24,bpp=32 ldb=sep0 \
video=mxcfb1:dev=ldb,LDB-XGA,if=RGB24,bpp=32 \
video=mxcfb2:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 \
root=/dev/nfs rw ip=192.168.1.104:192.168.1.235:192.168.1.1:255.255.255.0 fec_mac=13:32:43:34:21:43 nfsroot=192.168.1.235:/home/wucheng/rootfs,proto=tcp,nfsvers=3,nolock

2.信息

0 Kudos
Reply
4 Replies

2,548 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the IPU of imx6q in the Reference Manual, I don't think IPU can support HDMI 1080P@60 in your case,  for more detailed information, pls refer to the Reference Manual,

• Displays
• Five interfaces available. Total raw pixel rate of all interfaces is up to 532
Mpixels/sec, 24 bpp (266 Mpixels/sec per each IPU). Up to four interfaces may
be active at once.
• Two Parallel 24-bit display ports - up to 220 Mpixels/sec each (e.g. WUXGA+
@ 60Hz), or dual HD1080 + WXGA @ 60Hz.
• LVDS serial ports: One port up to 165 Mpixels/sec or Two ports up to 85
MP/sec (e.g. WUXGA+ @ 60Hz) each
• HDMI 1.4 port
• MIPI/DSI, 2 lanes @ 1 Gbps

0 Kudos
Reply

2,548 Views
wumr
Contributor I

是从否支持1024的双LVDS屏+HDMI1920x1080?

pastedImage_2.png

0 Kudos
Reply

2,548 Views
joanxie
NXP TechSupport
NXP TechSupport

"是从否支持1024的双LVDS屏+HDMI1920x1080?" what's difference from your orignal question? your orginal setting is dual lvds 1024 + HDMI 1080p, I don't think IPU can support your orginal settings

0 Kudos
Reply

2,548 Views
joanxie
NXP TechSupport
NXP TechSupport

“”是从否支持1024的双LVDS屏+HDMI1920x1080?“” what's difference between this from your original resolution? 

0 Kudos
Reply