Recently many customers faced the issue about connecting the git.freesacle .com failed when they built old bsp version like 4.1.15 or 3.14.52, when the customer repo init according to the yocto user guide, they get the error message like :
repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth
manifests:
escale.com[0: 192.88.156.202]: errno=Connection refused
fatal: cannot obtain manifest git://git.freescale.com/imx/fsl-arm-yocto-bsp.git
/////
git clone git://git.freescale.com:9418/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga
Cloning into 'fsl-arm-yocto-bsp'...
fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection refused
the reason is that the old bsp source code was moved to "https://source.codeaurora.org/external/imx", customer needs to change "git://git.freescale.com/imx" to "https://source.codeaurora.org/external/imx", for new repo init commands, try to use the commands like “repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b <branch> [-m <manifest>]”
for example:
4.1.15_1.0.0:
repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1.15-1.0.0_ga
4.1.15_2.0.0:
repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth -m imx-4.1.15-2.0.0.xml
4.1.15_2.1.1:
repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth -m imx-4.1.15-2.1.1.xml
then you can "repo sync" and "bitbake", but some customers still has the connection error on building firmware-imx package, the error message like :
ERROR: firmware-imx-1_5.4-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/opt/yocto/fsl-release-bsp/downloads//git2/git.freescale.com.imx.imx-firmware.git'...
fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection refused
ERROR: firmware-imx-1_5.4-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://git.freescale.com/imx/imx-firmware.git;branch=master;destsuffix=/opt/yocto/fsl-release-bsp/fsl_build...'. Unable to fetch URL from any source.
this reason is that 4.1.15 needs to download git2 package from git.freescale.com, then I uploaded the firmwar-imx git2 package, try to unzip first, then put packages under downloads/git2, then "bitbake firmware-imx" again