i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with i.MX 8/8X DDR initialization.  For more details, refer to the i.MX 8/8X main DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519   To reduce the number of attachments, older RPAs may be found in the attached zip file. Note: Devices with 17-row addresses (R0-R16) are not supported by this SoC.  ***IMPORTANT: For SCFWv1.7.0 and later, you must use the following RPA versions or later: MX8QXP_C0_B0_LPDDR4_RPA_1.2GHz_v16 MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v16 MX8QuadXPlus_DualXPlus_C0_B0_DDR3L_RPA_v22 MX8DualX_C0_B0_DDR3L_RPA_v20 Older versions of the RPA are not aligned to SCFWv1.7.0 and later.  If trying to use an older version of an RPA with SCFWv1.7.0, it will cause the SCFW not to boot.  The offending lines in the DCD output are as follows: For MX8QXP/DualX: DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ If the user wishes to use an older RPA with SCFW 1.7.0 and later (not recommended), then the above lines must be removed from older RPA DCD file outputs.  In addition, wrapping these lines are "#ifndef SCFW_DCD", "#else", and "#endif" preprocessor commands.  These should be removed as well.  For example of MX8QXP: [remove] #ifndef SCFW_DCD [remove] -/* For 1200MHz DDR, DRC 600MHz operation */ [remove] DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ [remove] #else <keep code as is> [remove] #endif
View full article
To enable USB 2.0 port on BB for USB OTG, you need to apply below two changes: device/fsl.git   diff --git a/imx8q/mek_8q/init.usb.rc b/imx8q/mek_8q/init.usb.rc index af4e388..0f3ab0b 100644 --- a/imx8q/mek_8q/init.usb.rc +++ b/imx8q/mek_8q/init.usb.rc @@ -44,7 +44,7 @@ on early-boot      mount functionfs mtp /dev/usb-ffs/mtp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      mount functionfs ptp /dev/usb-ffs/ptp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      setprop sys.usb.mtp.device_type 3 -    setprop vendor.usb.config "5b110000.usb3" +    setprop vendor.usb.config "ci_hdrc.0"      write /sys/module/libcomposite/parameters/disable_l1_for_hs "y"      symlink /config/usb_gadget/g1/configs/b.1 /config/usb_gadget/g1/os_desc/b.1   vendor/nxp-opensource/kernel_imx.git           revert below patch:           commit 2f9586c120971312e61df464264993899cf34536           Author: yang.tian <[email protected]>           Date:   Tue Jan 7 13:30:02 2020 +0800       MA-15242 Set usb2.0 port as usb host only for mek_8q  
View full article
The Guide is how to use Ubuntu filesystem with i.MX8 series platform.At present, I had try it on i.MX8QXP with 4.14.98 kernel with ubuntu16.04. The Document will be continuously updated with enable VPU, ubuntu18.04. The desktop we can chose Gnome or weston.  Because driver  support issue, gc7000 series gpu not support render Gnome destop but it can render weston destop.  Update 2019/7/31: Ubuntu-i.MX8-weston.pdf   Feature: weston + ubuntu18.04 + 4.14.98 kernel VPU (enable with gplay or gst-play)  GPU (could render desktop and run GPU demo under root privileges on Weston Desktop) I also try ubuntu with gnome desktop, ubuntu18.04 can not run gnome, need use ubuntu19.04. But Gnome Desktop just render by CPU.  ------------------------------------------------------------------------------------- Update 2020/3/6: Ubuntu-i.MX8M.pdf Just a simple guide for IMX8M series, will be  continuously updated. 
View full article
Multicore programming guide with Linux 3.14.52_1.1.0 and FreeRTOS BSP for i.MX 6SoloX
View full article
NOTE: Please suggest bitbake commands you find it useful! bitbake command Description bitbake <image> Bake an image (add -k to continue building even errors are found in the tasks execution) bitbake <package> -c <task> Execute a particular package's task. Default Tasks names: fetch, unpack , patch , configure , compile , install , package , package_write , and build. Example: To (force) compiling a kernel and then build, type: $ bitbake  linux-imx -f -c compile $ bitbake linux-imx bitbake <image > -g -u depexp Show the package dependency for image. Example: To show all packages included on fsl-image-gui $ bitbake fsl-image-gui -g -u depexp NOTE: This command will open a UI window, so it must be execute on a console inside the host machine (either virtual or native). bitbake <package> -c  devshell Open a new shell where with neccesary system values already defined for package hob bitbake frontend/GUI. bitbake <package> -c listtasks List all tasks for package bitbake virtual/kernel -c menuconfig Interactive kernel configuration bitbake <image> -c fetchall Fetch sources for a particular image bitbake-layers show-layers Show layers bitbake-layers show-recipes "*-image-*" Show possible images to bake. Without "*-images-*", it shows ALL recipes bitbake -g <image> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq Show image's packages bitbake -g <pkg> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq Show package's dependencies bitbake –v <image> 2>&1 | tee image_build.log Print (on console) and store verbose baking bitbake -s | grep <pkg> Check if certain package is present on current Yocto Setup
View full article
  Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 family developement board https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false  
View full article
Attached is an application note for iMX6 TVIN use case, some internal review was done. 2016-10-08, change it to pdf file.
View full article
Following docs(English or Chinese version) are also can be referred as a hand on guide. Freescale i.MX6 DRAM Port Application Guide-DDR3 飞思卡尔i.MX6平台DRAM接口高阶应用指导-DDR3篇   Please find i.Mx6DQSDL LPDDR2 Script Aid through below link. i.Mx6DQSDL LPDDR2 Script Aid  Please find i.Mx6DQSDL DDR3 Script Aid through below link. i.MX6DQSDL DDR3 Script Aid  Please find i.MX6SX DDR3 Script Aid through below link. i.MX6SX DDR3 Script Aid  Please find i.MX6SL LPDDR2 Script Aid through below link.. i.MX6SL LPDDR2 Script Aid  Please find i.MX6UL DDR3 Script Aid through below link. I.MX6UL DDR3 Script Aid  Please find i.MX6UL LPDDR2 Script Aid through below link. i.MX6UL_LPDDR2_Script_Aid  Please find i.MX6ULL LPDDR2 Script Aid through below link. i.MX6ULL_LPDDR2_Script_Aid 
View full article
To disable the Android dm-verity in the new devices you should have the below. A Window/Linux computer The Android SDK platform-packages tools. Download the Android Packages tool. To use the Android kernel or give root access to your Android device, it is needed to have some tools from the Android SDK like ADB or fastboot. To download those tools just go to below web-page: https://developer.android.com/studio#downloads Go to the “command line tools only” part and download the sdk-tools-windows-4333796.zip package. Note: Is recommended to store the content of the zip file in path that you could find without any problem since the Android SDK tools can only be run by the terminal console.   Unlock your Android device. On the Android GUI go to Settings -> systems -> About Phone At the bottom, you should see the build number of your Android device. Tap it multiple times until appears on the screen that you are a developer now. Go to the developer options and search for the OEM unlock option. You need to activate that option. Open the power-shell terminal and go to the path where you stored the zip file.   Example for Windows: cd C:\users\diego\Documents\platform-tools‍ Then you will use the ADB tool (Adroid Debug Bridge). To use it you need to run adb.exe in your power-shell terminal. To run an executable in the Windows terminal is just with ".\". Connect the serial download cable to the host computer (the Type C for the i.MX8M and i.MX8MM. The OTG for the i.M6 SabreSD boards). Open the adb server. .\adb.exe start-server‍ See your connected devices. .\adb.exe devices‍ You should see your device and the serial number that is assigned to the device. Then, enter into Bootloader mode. .\adb.exe reboot bootloader‍       Note to see if your board successfully entered to Bootloader mode. In your serial terminal, you should see that you are in Bootloader mode. Once inside the Bootloader mode, using fastboot you can unlock your phone. First, see if your computer recognizes your board once inside the Bootloader mode. .\fastboot.exe devices‍ If you do not see any device, go to Appendix A of the document. Finally, Unlock and reboot the board. .\fastboot.exe oem-unlock .\fastboot.exe reboot‍‍         Unlock the dm-verity option. After the board rebooted. Start again the adb server .\adb.exe start-server .\adb.exe devices‍‍ Then root the board .\adb.exe root ‍ After rooting the board, disable the dm-verity option .\adb.exe disable-verity‍ After disabling the verity option, it will request you to reboot your board. Just reboot your board. .\adb.exe reboot ‍ With that, you should have successfully disabled the verity option on your board.   Appendix A Update the USB driver (For Windows only) If your computer does not recognize once you are inside the bootloader mode. What you need to do is update the USB driver. To update the driver, follow the below steps. First, open your device manager and locate the Universal Serial Bus devices -> USB download gadget. Then press the right-click and select the Update driver option. Select the “Browse my computer for driver software” option. Select the “Let me pick from a list of available drivers on my computer” option.     Select the ADB Device Model.   And accept to install the driver. After that, your computer should recognize the board being into Bootloader mode.   Appendix B connects your Android device to a Linux computer through ADB.   You could face some adb problems if you want to connect your Android device to a Linux computer. If you want to use adb, the Android image does not allow you due to a permission problem. To make it work, you need to create a new rule for a plug device. To make the new rule, create a document inside the /etc/udev/rules.d named 51-android.rules. Inside the document write the following:   SUBSYSTEM=="usb", ATTR{idVendor}=="18d1", ATTR{idProduct}=="d002", MODE="0660",  GROUP="plugdev", SYMLINK+="android%n"‍‍   Where the ATTR{idVendor} and ATTR{idProduct} is the USB id for the board. To know that information. Write lsusb and your Android device is the one named Google Inc. Then reboot your computer. With this new rule, ADB should work as usual. Hope this document could be useful to someone. Best regards, Diego.
View full article
adv7180 is the 8 bits parallel CSI interface TVin to iMX8QXP validation board. Its weaving mode de-interlace can be supported on both iMX8QXP B0 and C0 chips, but blending mode de-interlace can only work on iMX8QXP C0 chips.   ISL79987 is the 4 virtual channel TVin chip which can input 4 CVBS cameras to iMX8QXP with MIPI CSI2 inteface, it can only work with iMX8QXP C0 chips. The iMX8QXP B0 chips have MIPI CSI2 virtual channel errata.   To test the capture to file: $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -num 300 -fmt YUYV -of   To test the preview on screen: $ killall weston $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -fmt RGBP -num 30000   Note: 1. For weaving mode de-interlace, when the ISI is doing de-interlace, it can't do CSC at the same time, so preview will get color issue, because the real output video is always YUYV format. 2. For blending mode de-interlace, it must use ISI0, so for ISL79987, only one camera can use blending mode, the other three cameras are still using weaving mode. The preview color is OK for such use case. 3. The patch is for L4.19.35 BSP.     2019-11-14 update: Add the test application "mx8_v4l2_cap_drm.tar.gz" to support YUYV render to display. Test command to render 4 weaving mode cameras:    ./mx8_v4l2_cap_drm.out -cam 0xF -fmt YUYV -num 30000     2020-04-29 update: Add "0006-isl7998x-fix-the-mipi_bps-overwrite-issue-from-set_f.patch", it fixed the issue that MIPI bps information in isl7998x_data->format.reserved[0] had been overwritten by isl7998x_set_fmt().   2021-06-11 update: Added the patches based on L5.4.70_2.3.0 GA BSP.
View full article
In order to improve the speed of compilation, VMWare Player 14.0 is installed on local hard disk, and Ubuntu 18.04 LTS is installed on a SSD with at least 500GB size and USB3.1 specification. When installing ubuntu 18.04 LTS to SSD, it should be allocated at least 350GB of disk space, because compiling this version of android requires a larger disk space. The following are detailed compilation steps: Part l Configuring Ubuntu 18.04 LTS 1. Installing Ubuntu 18.04 on VMplayer 14.0 After installation is done, root user should be set at first. # sudo passwd root Then follow these steps to configuration ubuntu 18.04 for environment of compiliation --Changing sources of ubuntu 18.04 mirror If you are Chinese users, you can do the step, which can improve your system performance. # sudo cp /etc/apt/sources.list /etc/apt/sources.list.bak # sudo geit /etc/apt/source.list Comment I.MX customers outside China do not need to modify Ubuntu source list, or can modify it to local mirror site of Ubuntu 18.04, which can improve the speed of software upgrade.    Delet all sources and copy following lines here, Then save it and exit Changing ubuntu source deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse    Then running these 2 commands to update sources and packages    # sudo apt-get update    # sudo apt-get upgrade 2. Installing packages for compiliation Packages for compiliation # sudo apt-get install flex bison gperf build-essential zlib1g-dev lib32ncurses5-dev x11proto-core-dev libx11-dev lib32z1-dev libgl1-mesa-dev tofrodos python-markdown libxml2-utils xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 gcc-multilib g++-multilib subversion openssh-server openssh-client uuid uuid-dev zlib1g-dev liblz-dev lzop liblzo2-2 liblzo2-dev git-core curl # sudo apt-get install u-boot-tools mtd-utils android-tools-fsutils openjdk-8-jdk device-tree-compiler aptitude libcurl4-openssl-dev nss-updatedb # sudo apt-get install chrpath texinfo gawk cpio diffstat gdisk m4 libz-dev libssl-dev Part 2 Compiling Android Q10.0.0_2.1.0 BSP 1. Downloading NXP source code for Android Q10.0.0_2.1.0    File name is imx-android-10.0.0_2.1.0.tar.gz.    Copy the file to ~/, and decompress it.    # cd ~/    # tar zxvf ./imx-android-10.0.0_2.1.0.tar.gz    Then “imx-android-10.0.0_2.1.0” directory is created at ~/, now run the command to download android source code. # source ./imx-android-10.0.0_2.1.0/imx_android_setup.sh Comment imx_android_setup.sh is a script file, which includes all steps needed by the environment of android Q10.0.0_2.1.0 BSP. If network environment is enough good, several hours later, it will be done. 2. Compiling Android Q10.0.0_2.1.0 Referring to steps in Android_User's_Guide.pdf, We summaries steps for compilation here: (1) Preparing cross-compile tool chain    In Android_User's_Guide.pdf, 2 kinds of tool chain are recommended for users. --- gcc-arm-8.3-2019.03-x86_64-aarch64-elf.tar.xz --- gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz    Users can select one of them, and then decompress it to /opt/ directory. On how to download them or more details, see Android_User's_Guide.pdf, page 3. Here we will use gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz as tool chain. (2) Beginning to Compile Android Q10.0.0_2.1.0 BSP    Since this version of Android BSP requires high memory capacity when compiling, if the memory configuration of the virtual machine is incorrect, it is very likely to cause the compilation to fail. The following is a list of variable tests for user reference: # cd android_build # export AARCH64_GCC_CROSS_COMPILE=/opt/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/aarch64-linux-gnu- # source build/envsetup.sh # lunch evk_8mp-userdebug # ./imx-make.sh -j2 2>&1 | tee build-log.txt Part 3 Errors During Compilation 1. Allocating 8GB Memory For VMware Player # ./imx-make.sh -j1 2>&1 | tee build-log.txt 2. Allocating 12GB Memory For VMware Player # ./imx-make.sh -j4 2>&1 | tee build-log.txt # ./imx-make.sh -j4 2>&1 | tee build-log.txt (Run it again) # ./imx-make.sh -j4 2>&1 | tee build-log.txt (Run it again)       So if we use 4 thread to compile BSP, command for compilation will have to be run for 3 times. NXP TIC Team Weidong Sun 2020/4/30
View full article
Platform: i.MX8QXP/8QM OS: Linux Supported Camera Modules: Max9286 + Max9271 + OV10635, Default BSP Max9286 + Max96705 + AR0144, patch Max9286 + Max96705 + OV9284, patch Max9286 + Max96705 + AP0101 + AR0132, patch NVP6324 + NVP2431 + IMX225, patch TP2855 + TP3812 + IMX307, patch ISL7998x + NTSC/PAL Sensor, patch adv7180 + NTSC/PAL Sensor, patch Detailed description in the attachment.
View full article
    Xenomai is real-time framework, which can run seamlessly side-by-side Linux as a co-kernel system, or natively over mainline Linux kernels (with or without PREEMPT-RT patch). The dual kernel nicknamed Cobalt, is a significant rework of the Xenomai 2.x system. Cobalt implements the RTDM specification for interfacing with real-time device drivers. The native linux version, an enhanced implementation of the experimental Xenomai/SOLO work, is called Mercury. In this environment, only a standalone implementation of the RTDM specification in a kernel module is required, for interfacing the RTDM-compliant device drivers with the native kernel. You can get more detailed information from Home · Wiki · xenomai / xenomai · GitLab       I have ported xenomai 3.1 to i.MX Yocto 4.19.35-1.1.0, and currently support ARM64 and test on i.MX8MQ EVK board. I did over night test( 5 real-time threads + GPU SDK test case) and stress test by tool stress-ng on i.MX8MQ EVK board. It looks lile pretty good. Current version (20200730) also support i.MX8MM EVK.     You need git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-4.19.35-1.1.0-20200818 (which inlcudes all patches and bb file) and add the following variable in conf/local.conf before build xenomai by command bitbake xenomai.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch. The following is test result by the command (/usr/xenomai/demo/cyclictest -p 99 -t 5 -m -n -i 1000  -l 100000😞 //Over normal Linux kernel without GPU SDK test case T: 0 ( 4220) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 9 Max: 23 T: 1 ( 4221) P:99 I:1500 C: 66672 Min: 7 Act: 10 Avg: 10 Max: 20 T: 2 ( 4222) P:99 I:2000 C: 50001 Min: 7 Act: 12 Avg: 10 Max: 81 T: 3 ( 4223) P:99 I:2500 C: 39998 Min: 7 Act: 11 Avg: 10 Max: 29 T: 4 ( 4224) P:99 I:3000 C: 33330 Min: 7 Act: 13 Avg: 10 Max: 26 //Over normal Linux kernel with GPU SDK test case T: 0 ( 4177) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 11 Max: 51 T: 1 ( 4178) P:99 I:1500 C: 66673 Min: 7 Act: 12 Avg: 10 Max: 35 T: 2 ( 4179) P:99 I:2000 C: 50002 Min: 7 Act: 12 Avg: 11 Max: 38 T: 3 ( 4180) P:99 I:2500 C: 39999 Min: 7 Act: 12 Avg: 11 Max: 42 T: 4 ( 4181) P:99 I:3000 C: 33330 Min: 7 Act: 12 Avg: 11 Max: 36   //Cobalt with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M --timeout 600s --metrics-brief T: 0 ( 4259) P:50 I:1000 C:3508590 Min:      0 Act:    0 Avg:    0 Max:      42 T: 1 ( 4260) P:50 I:1500 C:2338831 Min:      0 Act:    1 Avg:    0 Max:      36 T: 2 ( 4261) P:50 I:2000 C:1754123 Min:      0 Act:    1 Avg:    1 Max:      42 T: 3 ( 4262) P:50 I:2500 C:1403298 Min:      0 Act:    1 Avg:    1 Max:      45 T: 4 ( 4263) P:50 I:3000 C:1169415 Min:      0 Act:    1 Avg:    1 Max:      22   //Cobalt without GPU SDK test case T: 0 ( 4230) P:50 I:1000 C: 100000 Min: 0 Act: 0 Avg: 0 Max: 4 T: 1 ( 4231) P:50 I:1500 C:   66676 Min: 0 Act: 1 Avg: 0 Max: 4 T: 2 ( 4232) P:50 I:2000 C:   50007 Min: 0 Act: 1 Avg: 0 Max: 8 T: 3 ( 4233) P:50 I:2500 C:   40005 Min: 0 Act: 1 Avg: 0 Max: 3 T: 4 ( 4234) P:50 I:3000 C:   33338 Min: 0 Act: 1 Avg: 0 Max: 5 //Cobalt with GPU SDK test case T: 0 ( 4184) P:99 I:1000 C:37722968 Min: 0 Act: 1 Avg: 0 Max: 24 T: 1 ( 4185) P:99 I:1500 C:25148645 Min: 0 Act: 1 Avg: 0 Max: 33 T: 2 ( 4186) P:99 I:2000 C:18861483 Min: 0 Act: 1 Avg: 0 Max: 22 T: 3 ( 4187) P:99 I:2500 C:15089187 Min: 0 Act: 1 Avg: 0 Max: 23 T: 4 ( 4188) P:99 I:3000 C:12574322 Min: 0 Act: 1 Avg: 0 Max: 29 //Mercury without GPU SDK test case T: 0 ( 4287) P:99 I:1000 C:1000000 Min: 6 Act: 7 Avg: 7 Max: 20 T: 1 ( 4288) P:99 I:1500 C:  666667 Min: 6 Act: 9 Avg: 7 Max: 17 T: 2 ( 4289) P:99 I:2000 C:  499994 Min: 6 Act: 8 Avg: 7 Max: 24 T: 3 ( 4290) P:99 I:2500 C:  399991 Min: 6 Act: 9 Avg: 7 Max: 19 T: 4 ( 4291) P:99 I:3000 C:  333322 Min: 6 Act: 8 Avg: 7 Max: 21 //Mercury with GPU SDK test case T: 0 ( 4222) P:99 I:1000 C:1236790 Min: 6 Act: 7 Avg: 7 Max: 55 T: 1 ( 4223) P:99 I:1500 C:  824518 Min: 6 Act: 7 Avg: 7 Max: 44 T: 2 ( 4224) P:99 I:2000 C:  618382 Min: 6 Act: 8 Avg: 8 Max: 88 T: 3 ( 4225) P:99 I:2500 C:  494701 Min: 6 Act: 7 Avg: 8 Max: 49 T: 4 ( 4226) P:99 I:3000 C:  412247 Min: 6 Act: 7 Avg: 8 Max: 53 //////////////////////////////////////// Update for Yocto L5.4.47 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.47 2.2.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP). You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git,  and git checkout xenomai-5.4.47-2.2.0. You need to add the following variable in conf/local.conf before build xenomai by command bitbake imx-image-multimedia.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.4.70 2.3.0  /////////////////////////////////////////////////////////// New release  for Yocto release L5.4.70 2.3.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP) and i.MX8QM/QXP. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.0. Updating: 1, Support i.MX8QM and i.MX8QXP 2, Fix altency's the issue which uses legacy API to get time   //////////////////////////////////////// update for Yocto L5.4.70 2.3.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-5.4.70-2.3.2. Updating: 1, Enable Xenomai RTDM driver in Linux Kernel 2, Currently CAN, UART, GPIO,  SPI and Ethernet (in debug for RTNet)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf to enable relative device in Xenomai domain, for example rt-imx8mp-flexcan.   //////////////////////////////////////// Update for Yocto L5.4.70 2.3.4  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.4. You need to git clone  https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.4. Updating: 1, Enable RTNet FEC driver 2, Currently CAN, UART, GPIO,  SPI and Ethernet ( FEC Controller)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf and KERNEL_DEVICETREE += " freescale/imx8mm-rt-ddr4-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mmddr4evk.conf to enable rt_fec device in Xenomai domain. Verifying the network connection by RTnet Ping Between i.MX8M Mini EVK and i.MX8M Plus EVK a, Setup test environment 1, Connect ENET1 of  i.MX8M Plus EVK (used as a master) and  ENET of i.MX8M Mini EVK (used as a slave) of  to a switch or hub 2, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Plus EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.101" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -65,7 +65,7 @@ TDMA_MODE="master" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 3, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Mini EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.102" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -59,13 +59,13 @@ STAGE_2_CMDS="" # TDMA mode of the station ("master" or "slave") # Start backup masters in slave mode, it will then be switched to master # mode automatically during startup. -TDMA_MODE="master" +TDMA_MODE="slave" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 4, rename imx8mm-rt-ddr4-evk.dtb to imx8mm-ddr4-evk.dtb in /run/media/mmcblk1p1,  rename imx8mp-rt-evk.dtb to imx8mp-evk.dtb in /run/media/mmcblk1p1, and reboot board. 5, Run the below command on i.MX8M Mini EVK board. cd /usr/xenomai/sbin/ ./rtnet start & 5, Run the below command on i.MX8M Plus EVK board. cd /usr/xenomai/sbin/ ./rtnet start & When you see the log (rt_fec_main 30be0000.ethernet (unnamed net_device) (uninitialized): Link is Up - 100Mbps/Full - flow control rx/tx) and you can run command "./rtroute" to check route table if the slave IP (192.168.100.102) is in route.. b, Verify the network connection using the command below: ./rtping -s 1024 192.168.100.102 //////////////////////////////////////// Update for Yocto L5.10.52 2.1.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.52 2.1.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.52-2.1.0. Updating: 1, Upgrade Xenomai to v3.2 2, Enable Dovetail instead of ipipe. Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" Notice: If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch.  Latency testing of Xenomai3.2+Dovetail with isolating CPU 2,3 ( Xenomai 3.2 on 8MM DDR4 EVK with GPU test case (GLES2/S08_EnvironmentMappingRefraction_Wayland) + iperf3 + 2 ping 65000 size + stress-ng --cpu 2 --io 2 --vm 1 --vm-bytes 256M --metrics-brief )😞 The following is test result by the command (/usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000) root@imx8mmddr4evk:~# /usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000 # /dev/cpu_dma_latency set to 0us policy: fifo: loadavg: 5.96 6.04 6.03 7/155 1349 T: 0 ( 615) P:50 I:1000 C:63448632 Min: 0 Act: 0 Avg: 0 Max: 55 T: 1 ( 616) P:50 I:1500 C:42299087 Min: 0 Act: 0 Avg: 1 Max: 43 T: 2 ( 617) P:50 I:2000 C:31724315 Min: 0 Act: 0 Avg: 1 Max: 51 T: 3 ( 618) P:50 I:2500 C:25379452 Min: 0 Act: 0 Avg: 1 Max: 53 T: 4 ( 619) P:50 I:3000 C:21149543 Min: 0 Act: 0 Avg: 1 Max: 47 //////////////////////////////////////// Update for Yocto L5.10.72 2.2.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.72 2.2.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.72-2.2.2. Updating: 1, Upgrade Xenomai to v3.2.1 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.15.71 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.15.71 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.15.71-2.2.0. Updating: 1, Upgrade Xenomai to v3.2.2 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai"   //////////////////////////////////////// Update for Yocto L6.1.55 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L6.1.55 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git recipes-rtlinux-xenomai -b Linux-6.1.x Updating: 1, Upgrade Xenomai to v3.2.4 and support i.MX93 2, Enable EVL (aka Xenomai 4) for i.MX93 and legacy i.MX(6/7D/8X/8M) Copy recipes-rtlinux-xenomai to <Yocto folder>/sources/meta-imx/meta-bsp/, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "evl" IMAGE_INSTALL:append += " libevl"   //////////////////////////////////////// Update for Yocto L6.6.52 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L6.6.52 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git recipes-rtlinux-xenomai -b Linux-6.6.52 Updating: 1, Upgrade Xenomai to v3.3 and support i.MX91/93/95 2, Upgrade EVL (aka Xenomai 4),  libevl to r50 and support i.MX91/93/95 Copy recipes-rtlinux-xenomai to <Yocto folder>/sources/meta-imx/meta-bsp/, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "evl" IMAGE_INSTALL:append += " libevl"    
View full article
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with MMDC initialization. The last sheet formats the register settings for use with ARM RealView ICE. It can also be used with the windows executable for the DDR Stress Test. This programming aid was used for internal NXP validation boards.
View full article
The iMX8QM LVDS has followed work mode, (There are two LVDS modules in IMX8QM): Single mode (LVDS panel connects to one channel) panel 1 and panel 2 can be different panels: Dual channel split mode (The panel needs two LVDS channels, CH0 for 1,3,5,7,... pixels and CH1 for 2,4,6,8,... pixels): Mirror dual mode (The two panels on same LDB PHY should be same panels on pixel clock and resolution, panel 1 and panel 2 are same; panel 3 and panel 4 are same): The reference patch is based on L5.4.3_GA1.0.0 BSP. LVDS single mode and dual channel split mode are supported in default Linux BSP. Patch 0002 can be used to test this dual mode on MEK board, some rework is needed on MEK board:     R194, R195, R208, R209, R213, R214 should be mounted. And the I6263 board can't be connected to LVDS0_CH0 and LVDS0_CH1 at the same time. The I6263 board can't be connected to LVDS1_CH0 and LVDS1_CH1 at the same time too. Note: for iMX8QXP, there is no mirror dual mode support, because its two LVDS ports are from two different LDB modules, there are no CH1 for them: Note: for iMX8QXP dual channel split mode (The pixel order can be switched: LDB1_CH0 for 1,3,5,7,... pixels and LDB2_CH0 for 2,4,6,8,... pixels; or LDB2_CH0 for 1,3,5,7,... pixels and LDB1_CH0 for 2,4,6,8,... pixels), iMX8QM LVDS has no such feature.
View full article
The document to descript change the u-boot environment variables under the Linux rootfs.  Also provide a demo on i.MX6ull evk of sdcard mirror.  Linux fw_printenv fw_setenv to access U-Boot's environment variables.pdf  --- the document fw_printenv_fw_setenv_demo_iMX6ullevk_L4.14.98_2.0.0_ga.sdcard  --- demo sdcard mirror
View full article
When working with an evaluation kit you will be provided with a System Controller Firmware (SCFW) binary included in your BSP. This scfw binary has been tailored for that specific board and you might need to modify some board dependencies to fit your specific hardware. This document aims to provide an overview on the SCFW porting process, for detailed information please refer to the System Controller Porting guide (sc_fw_port.pdf).   Setting up the system The SCFW is built on a Linux host. The steps to set-up your system are the following: Download the GNU ARM Embedded Toolchain: 6-2017-q2-update June 28, 2017 from the ARM website: Select a directory to untar the file unto, for instance: mkdir ~/gcc_toolchain cp ~/Downloads/gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2 ~/gcc_toolchain/ cd ~/gcc_toolchain/ tar xvjf gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   Set TOOLS environment variable to the directory containing the tool chain, "~/gcc_toolchain" on the example above, .bash_profile can also be modified to export this environment variable: export TOOLS=~/gcc_toolchain/ srec_cat is also necessary for the build, this is usually contained in the srecord package, on ubuntu you can do: sudo apt-get update sudo apt-get install srecord Now you can change to the porting kit directory (e.g. scfw_export_mx8qm) and build the scfw. System Controller Firmware Porting kit  The SCFW porting kit contains source files and object files that will allow you to modify the SCFW to work with your board. You can get the latest System Controller Firmware Porting kit from the i.MX Software and development webpage: Once you obtain the porting kit untar it: tar xvzf imx-scfw-porting-kit-1.1.tar.gz‍ You will see the following file structure: The porting kit is contained under packages, the README contains the instructions to extract the porting kit, basically: cd packages/ chmod a+x imx-scfw-porting-kit-1.1.bin ./imx-scfw-porting-kit-1.1.bin‍‍‍ You will be prompted to accept an End User License Agreement: Once you accept the agreement the porting kit will be extracted in a new folder, the folder structure is as follows: All documentation regarding SCFW is under doc/pdf or in html format if preferred, it is recommended to go over sc_fw_port.pdf. The porting kits for different SoC variants (QM A0, QM B0 and QXP B0) are under src packaged as tar.gz, all other files are SCFW libraries for different software packages, such as Linux, QNX, FreeRTOS, U-boot, ARM Trusted Firmware, etc...   If you will be working with several SoC variants (working with both QXP and QM) it is recommended to extract all porting kits into a single directory, that way you will be able to build for any variant from this directory, the command to do this is: cd imx-scfw-porting-kit-1.1/ cd src/ find scfw_export_mx8*.gz -exec tar --strip-components 1 --one-top-level=scfw_export_mx8 -xzvf {} \;‍‍‍ A scfw_export_mx8 folder will be created, from here you will be able to build SCFW for any supported variant. Or you can just extract the package for the variant you are interested on and use that. cd scfw_export_mx8/‍ All the build folders contain the results of building the SCFW and platform is where the source of the SCFW is stored.   All the code that is specific to a board configuration is under "platform/board/mx8<derivative>_<board_name>" where derivative is the i.MX8 silicon family such as QXP or QM, and board name is the name of the board the SCFW package is for. The first step in porting the SCFW to your board is to create a folder for your i.MX8 derivative and board, you can take one of the available board examples and rename the folder, that will provide you a project to get started with, for instance: cp -r platform/board/mx8qm_val/ platform/board/mx8qm_myBoard/‍‍‍‍‍‍‍‍‍‍ The board in this example will be called "myBoard" and it is for an i.MX8QM B0 device. To build a SCFW for this board simply call: make qm R=B0 B=myBoard‍‍‍‍‍‍‍‍‍‍‍‍ If the target is an i.MX8QXP simply take a board based on this device and change the call to "make qx". Additional information such as build options and in detailed boot information can be found in the SCFW porting guide (sc_fw_port.pdf), chapter 2 of this document is a great introduction to the porting process.   Overview and useful information Configuring the PMIC overview and board.c common modifications The main file that needs to be altered (if not the only) is the "board.c" file, it is located at "platform/board/mx8X_board/". The board.c file contains most of the board related information such as SCU UART ports, PMIC initialization routines, PMIC temperature alarms settings and you can also modify it to configure LDOs voltages and communicate with the PMIC in general. All functions in the board.c file are executed by the SCU itself and this gives you access to the I2C interface that is used to communicate with the PMIC. SoC resources that are powered by an external supply (PMIC LDO for instace) such as AP cores and GPUs are powered off/on by board_set_power_mode, the mapping of the resource to an specific PMIC supply happens in board_get_pmic_info, for instance in our i.MX8QM validation board using the A53 subsystem is powered by SW2 of the third PMIC (PMIC_2_ADDR addresses start at PMIC_0) on the PF100 PMIC card and by SW5 of the first PMIC (PMIC_0_ADDR) on the PF8100 PMIC card. case SC_SUBSYS_A53: pmic_init(); if (pmic_card == PF100) { pmic_id[0] = PMIC_2_ADDR; pmic_reg[0] = SW2; *num_regs = 1; } else {/* PF8100_dual Card */ pmic_id[0] = PMIC_0_ADDR; pmic_reg[0] = PF8100_SW5; *num_regs = 1; } break; ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The voltages of SoC resources that are powered by an external supply (AP cores, GPUs, etc...) are managed by board_set_voltage in the board.c file. The mapping of resource to power supply occurs in board_get_pmic_info as in the example above. Eight "board resources" (SC_R_BOARD_R0, ... SC_R_BOARD_R7) are available, these resources allow you to define components in your board that the SCU can manage, for instance a sensor on your board powered by one of the PMIC LDOs can be mapped to a board resource and the board.c file can be modified to power on/off the sensor as well as modifying its voltage. Modifying the voltage on a board resource can be either be done by modifying the voltage at board_trans_resource_power (see below) or if the voltage needs to change at run time the function board_set_control can be modified to change the voltage whenever a miscellaneous call (more details in the Miscellaneous Service 101) is made on that resource. For instance to change the voltage on SC_R_BOARD_R7 you would have the following case to board_set_control: case SC_R_BOARD_R7: if (ctrl == SC_C_VOLTAGE) { /* Example only PMIC_X_ADDR and PMIC_SUPPLY need to match an actual device */ pmic_interface.pmic_set_voltage(PMIC_X_ADDR, PMIC_SUPPLY, val, step); } else return SC_ERR_PARM; break;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The case above will be executed by the SCU every time the application calls the function below: sc_misc_set_control( ipc, SC_R_BOARD_R7, SC_C_VOLTAGE, voltage_val);‍‍‍‍‍‍‍‍ Powering on/off a board resource happens at board_trans_resource_power in the board.c file. For instance in NXP's validation board the PTN5150 on the board is managed through a board resource 0, and the power on/off is managed as follows: case BRD_R_BOARD_R0 : /* PTN5150 (use SC_R_BOARD_R0) */ if (pmic_ver.device_id == PF100_DEV_ID) { if (to_mode > SC_PM_PW_MODE_OFF) { pmic_interface.pmic_set_voltage(PMIC_2_ADDR, VGEN6, 3300, SW_RUN_MODE); pmic_interface.pmic_set_mode(PMIC_2_ADDR, VGEN6, VGEN_MODE_ON); } else { pmic_interface.pmic_set_mode(PMIC_2_ADDR, VGEN6, VGEN_MODE_OFF); } } else {/* PF8100_dual Card */ if (to_mode > SC_PM_PW_MODE_OFF) { pmic_interface.pmic_set_voltage(PMIC_1_ADDR, PF8100_LDO1, 3300, REG_RUN_MODE); pmic_interface.pmic_set_mode(PMIC_1_ADDR, PF8100_LDO1, RUN_EN_STBY_EN); } else { pmic_interface.pmic_set_mode(PMIC_1_ADDR, PF8100_LDO1, RUN_OFF_STBY_OFF); } } break;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Whenever the function below is called from the application side the SCU will execute the code above: sc_pm_set_resource_power_mode(ipc, SC_R_BOARD_R0, SC_PM_PW_MODE_ON/OFF);‍‍‍‍‍‍‍‍ board_config_sc is used to mark resources that the SCU needs, such as the I2C module and pads used to communicate with the PMIC, any resource needed by the board.c functions to work should be marked in this function as not movable, for instance to keep the SCU I2C module the following line is added: rm_set_resource_movable(pt_sc, SC_R_SC_I2C, SC_R_SC_I2C, false);‍‍‍‍‍‍‍‍‍ The following pads are part of the SCU and the application will not be able to access them: - SC_P_SCU_PMIC_MEMC_ON - SC_P_SCU_WDOG_OUT - SC_P_PMIC_EARLY_WARNING - SC_P_PMIC_INT_B - SC_P_SCU_BOOT_MODE0 through SC_P_SCU_BOOT_MODE5 board_system_config is where early resource management occurs, this function is only called when the alt_config flag is set in the image, and it can create partitions and allocate resources to it. More details are found in the resource management service 101. board_get_pcie_clk_src defines the clock that the PCIe uses, it can be either BOARD_PCIE_PLL_EXTERNAL or BOARD_PCIE_PLL_INTERNAL. board_print is very useful to debug your changes the syntax is as follows: board_print(3, "Debug printout %d\n", val);‍‍‍‍‍‍‍ Where the first parameter is the Debug Level and from there on it works as a standard printf. The output will only be visible on the SCU debug output whenever the SCU is built with the corresponding debug level, in the case above the SCFW needs to be built as follows in order to see the output: make qm B=myBoard‍‍‍‍ DL=3 or higher (debug level goes from 0 to 5)‍‍‍‍‍‍‍   Usage examples The following utility shows how to make System Controller Firmware requests and provides a way to make such requests through command line interface on both QNX and Linux System Controller Firmware Command Line Utility for Linux and QNX   System Controller Firmware 101  
View full article
I²C is a communication protocol used to exchange information between cores. To see more about I²C, please follow this link Wikipedia:I²C. Enable I2C-tools in LTIB into Package List: Reboot your file system, there are three new I²C commands: i2cdetect, i2cdump and i2cset. All examples below were tested in a iMX27ADS, but this programs seems to have the same behavior to all platforms. Detecting busses This command lists all installed bus. mx27# i2cdetect -l i2c-0   unknown         MXC I2C Adapter                         Algorithm unavailable There is one installed bus with address 0. Installed Chips I2cdetect shows the installed chips too. mx27# i2cdetect 0     WARNING! This program can confuse your I2C bus, cause data loss and worse!     I will probe file /dev/i2c/0.     I will probe address range 0x03-0x77.         0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f 00:          XX XX XX XX XX XX XX XX XX XX XX XX XX 10: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX 20: XX XX XX XX XX XX XX XX XX XX XX XX XX 2d XX XX 30: UU XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX 40: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX 50: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX 60: XX XX XX XX XX XX XX XX XX XX UU XX XX XX XX XX 70: XX XX XX XX XX XX XX XX There are several cores installed into bus i2c-0. If you received an error message like this: # i2cdetect 0 Error: Could not open file `/dev/i2c-0' or `/dev/i2c/0': No such file or directory You will need to create the special file /dev/i2c-0 : # mknod /dev/i2c-0 c 89 0 Chip Registers i2cdump shows a list of all registers for a core. For example, the command above shows registers for core with address 0x6a: mx27# i2cdump 0 0x6a No size specified (using byte-data access)     WARNING! This program can confuse your I2C bus, cause data loss and worse!     I will probe file /dev/i2c/0, address 0x6a, mode byte         0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef 00: 00 00 28 00 00 03 15 03 00 00 00 00 00 00 03 01    ..(..???......?? 10: 04 01 00 00 04 01 00 00 17 41 1d 00 09 09 1f 03    ??..??..?A?.???? 20: 00 00 40 00 08 00 0c 00 0f 01 00 00 00 00 08 11    ..@.?.?.??....?? 30: 00 0f 05 fe 0b 00 00 00 82 00 0c 02 00 00 01 00    .????...?.??..?. 40: 21 f0 7c 1f 00 00 01 00 7a 40 80 38 00 01 47 00    !?|?..?.z@?8.?G. 50: 3c 00 17 21 1b 1b 24 9f 00 3e 0f 0f 60 05 cd 03    <.?!??$?.>??`??? 60: 89 04 89 01 02 00 0a 05 00 19 ff 03 24 0f 78 00    ?????.??.?.?$?x. 70: 00 b2 06 14 04 08 00 a3 c8 15 05 15 3c 00 00 20    .?????.?????<.. 80: 07 2f 07 00 00 00 00 00 00 00 00 ff 03 1a 1a 1a    ?/?.........???? 90: 1a 1a 40 03 00 00 00 00 00 00 00 00 00 00 e4 00    ??@?..........?. a0: 00 02 4d 00 96 00 1d 00 a0 00 db 00 7e 00 00 00    .?M.?.?.?.?.~... b0: 00 00 00 00 00 00 f0 00 00 00 00 00 00 00 00 00    ......?......... c0: 00 00 00 00 48 9c 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a    ....H??????????? d0: 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a    ???????????????? e0: 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a    ???????????????? f0: 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a 1a    ???????????????? Setting a register To change some register value, use i2cset like in example below: mx27# i2cset 0 0x6a 01 0x0008 w     WARNING! This program can confuse your I2C bus, cause data loss and worse!     I will write to device file /dev/i2c/0, chip address 0x6a, data address     0x00, data 0x08, mode word. Value 0x8 written, readback matched Where: 0 is the bus address 0x6a is the slave address 01 is the register address 0x0008 is the new value for register w is the word mode for the setting
View full article
This documents describes the neceesary steps to set up Qt Creator with the Qt5 toolchain that is available as part of the 3.14.28 BSP Release. Requirements 1) Linux machine. Ubuntu 12.4 or higher is recommended. 2) Yocto Freescale BSP Release L3.14.28 or higher. For this example we'll use the Freescale BSP Release L3.14.28 but you may use future BSP releases that include the Qt toolchain. - Freescale BSP Release Documentation L3.14.28 (login required) https://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&location=null&fpsp=1&WT_TYPE=Supporting%20Information&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=gz&WT_ASSET=Documentation&fileExt=.gz&Parent_nodeId=1337637154535695831062&Parent_pageType=product&Parent_nodeId=1337637154535695831062&Parent_pageType=product 3) Qt5 Meta Toolchain (Poky 1.7 qt5 / L3.14.28 for our example but you may use the qt toolchain that corresponds to the BSP that will be used) For information on how to extract and install the meta toolchain please follow the steps on the next document but with the following command: $ bitbake meta-toolchain-qt5 https://community.freescale.com/docs/DOC-95122 Task #7 - Create the toolchain Then run the script. fsl-release-bsp/<BUILD_DIR>/tmp/deploy/sdk/poky-glibc-x86_64-meta-toolchain-qt5-cortexa9hf-vfp-neon-toolchain-1.7.sh Installing Qt Creator We will use the Open Source version of Qt Creator. Please make sure that your application does comply with the requirements of Open Source Software before installing. You may download Qt Creator Open Source for Linux from the following link: http://www.qt.io/download-open-source/ Once you downloaded the installer you will need to make sure that the file has permission to be executed. You can add this with the following command: $ chmod +x qt-unified-linux-x64-2.0.2-2-online.run Then run the installer $ ./ qt-unified-linux-x64-2.0.2-2-online.run After the information from the repositories has been fetched you will be asked where to install Qt Creator. Then you will be asked which components to install. We will install Qt 5.4 which is the one supported on the 3.14.28 BSP release. You will need to accept the License Agreement and then the installer will fetch and install the necessary files. Configuring Qt Creator Once it’s finished downloading, launch Qt Creator. You can do this with the following command: cd <INSTALATION_DIR>/Tools/QtCreator/bin $./qtcreator.sh Under the Tools top bar menu, chose Options… On the Options window’s left menu chose Build & Run and then the Compilers tab and select Add GCC. On the next screen chose a name for this Compiler (i.e. i.MX Qt5) and then select the Compiler path, which may vary depending on where you have it installed but by default should be in: /opt/poky/<VERSION>/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++ It should then be detected as arm-linux on the ABI section. Next select the Qt Versions tab and click on Add… Look for the qmake on the toolchain path, which is by default: /opt/poky/<VERSION>/sysroots/x86_64-pokysdk-linux/usr/bin/qt5/qmake Finally, on the Kits tab add a new kit and select the sysroots from the toolchain, which is by default located in: /opt/poky/<VERSION>/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi Qt Creator is now configured for building for the i.MX6.
View full article